This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Horatiu said:the popular but outdated SSD1963 controller
SSD1963 did not capture too many, "cell phone sockets" did it? Might that speak to the absence of SSD replacement?
Your 800x480 TFT seems a bit "pixel sparse" does it not? (realize that cell phones, 5/7 or 4.3/7 that size - often have 2x+ that number pixels!)
Was the MCU you've chosen (really) designed to accommodate that size/capacity TFT? This maker - others - have superior MCUs - with greater emphasis placed upon the TFT interface.
Pushing a large rock - "up" a tall hill - using (only) your nose - can be done. Is it worthwhile? (may warrant your consideration...)
Amit Ashara said:Internal RAM is going to be limitation for most of them (if not all).
My reply placed no restrictions upon the "extent" of TFT drive solution. Suggested was the "modeling" of the techniques/components/methods of those w/maximum experience & success in TFT application. (that clearly - cell & tablet makers)
Poster should be prepared for extremely S L O W screen updates - noticeably so - especially when compared to cell or tablet! Your users will notice - and squawk (as they should) of that I assure you!
May prove worthwhile for you to procure & gut a "lesser" tablet (which you can acquire in volume) and see if that can be "massaged" into service. Parts w/in will always (far) exceed those resident - this forum.
Amit Ashara said:Jump start rather than to reinvent the wheel.
Thank you - your firm, others produce MCUs far more oriented toward "real" TFT control/management. Forcing Cortex M4s into this role (almost always) fails to meet user expectations. (users will "naturally" compare to cells/tablets - where up-scale MCUs reign - M4s "have no chance!")
This is an unfortunate - yet very strong/impacting - reality! Unless the screen will (primarily) be used for, "Fixed images" or text selections - the update speed will be most notable - and will be rejected! (imho - yet I'm past co-founder of public display firm...)
Poster (thus far) seeks to combine a, "pixel-starved" screen with a, "SLOW (in comparison) screen update MCU" - that's sure to Sell!
Look even at TV - larger screens - even more pixels - and 120Hz. (some even faster!)
That's the strong trend - again reality - and M4 (despite the LCD add-on) may not prove, "best/brightest." (to be kind)