This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PinMux-Software

Other Parts Discussed in Thread: HALCOGEN

Tiva C Series PinMux Utility.

I´m currently working with the PinMux tool. It seems for me that the tool just supports a part of the configuration (so the tool is not really helpful for me). Example 1: I can enable the EPI bus but I can't define the bus type and the bus size. Example 2: I can enable the USB controller but I can't disable the ULPI feature. Example 3: I can enable a GPIO but I can't enable the interrupt for the GPIO. Is there a newer version of the program in the pipeline which supports these features?]

 

  • Hello Heinz,

    The tool is for IO Mapping only and not for Peripheral configuration (unlike Grace or Halcogen). The next version of the tool with the bug fixes are in the pipe and there is no immediate plans for a Graphical Tool for Peripheral Configuration Yet.,

    Regards
    Amit