Other Parts Discussed in Thread: HALCOGEN
I've generated the code using HalCoGen, to interrupt on both edges (rising an falling) of three HET input pins. Code works perfectly well as long the input signals are not changing at the same time.
If two input signals generating Edge 0 and Edge 2 interrupts are in phase, Edge 0 interrupt is still triggered while Edge 2 is not.
What needs to be changed in the HET setup to be able to trigger interrupts when Edge 0 and Edge 2 are changing at the same time?
Please advice.