Other Parts Discussed in Thread: TM4C123GH6PM
Hi,
I am using a tm4c123gh6pm µcontroller and the LS027B7DH01LCD LCD Display. I am trying to use the TvaWare graphics library, but I am having some understanding problems how to correctly use the library. Right now I am trying to draw an image onto my display, the problem is that i don't really know how I'm supposed to do this. You can see the programm below.
#define SCRBUF_ZEILEN 400
#define SCRBUF_ZEILEN_LEN 50
#define SCRBUF_SIZE SCRBUF_ZEILEN_LEN*SCRBUF_ZEILEN
GrContextInit(&Context, &Display);
Context.i32Size = SCRBUF_SIZE;
Display.ui16Height = 240;
Display.ui16Width = 400;
/*
sRect.i16XMin = 0;
sRect.i16YMin = 0;
sRect.i16XMax = 100;
sRect.i16YMax = 100;
GrContextForegroundSet(&Context, ClrBlack);
GrRectFill(&Context, &sRect);
*/
GrImageDraw(&Context, ImageBuffer, 15, 15);
//GrFlush(&Context);
I'm not really sure if this is correct, but i declared both Context and Display globally. I'm also not so sure about the ImageBuffer array, do I have to write IMAGE_FMT_1BPP_COMP, in the array. I also don't understand the purpose of the void * pvDisplayData, I read that it points to a driver specific display driver, but what are those and do I need them?
If somebody can help me use the graphics library, I would be really thankful.
I would really appreciate help.
Best regards