Other Parts Discussed in Thread: HALCOGEN
i worked with example codes in halcogen software. the program was build successfully without error.
while configuring i used hardware raising edge trigger with GPIOB 0 and selected the pin 0 and 1 in channel one
can i give square pulse input for GPIOB 0 to trigger and sine wave input to ADC channel 1 (pin 0 (positive) and pin 1 (negative) from signal generator for testing purpouse.
thanks and regards
K.Manjunathan
PSGIAS