Other Parts Discussed in Thread: TMS570LS3137, HALCOGEN
Hello.
I'm using a TMS570LS3137 with a Micrel KSZ8895RQI attached over RMII. I've already learned that the RMII_RXER line is optional, and so I want to use this pin (N19) as GPIO for a chip select line. This line is most of the time high and I can't get a connection. If I set it to low permanently the connection is working.
I've used HalCoGen 03.06.00 Pinmux to set this pin to AD1EVT function.
Is there a chance to use it this way? Can the MAC in the TMS570LS3137 ignore the RMII_RXER pin?
Best Regards
Christian