Other Parts Discussed in Thread: TM4C123GH6PM, TM4C123FE6PM
Hi,
Background:
I am looking for a TM4C processor with the following features:
- M3/M4 Core
- 2 CAN transceivers
- <10mA peak run current @10-20MHz
- Flash 128K to 256K
- RAM 32K-64K
Things that I've done:
- I have been looking into TM4C123XX family datasheets and I came across TM4C123GH6PM and TM4C123FE6PM. They meet all the specs except for <10mA peak run current consumption
Question:
1. Is there a TM4C processor that meets all the specifications?
Thank you in advance.
Rifat Sheikh