Other Parts Discussed in Thread: TMS570LC4357, HALCOGEN, UNIFLASH
Hi TI,
In HalcoGen I generate FREERTOS Project for TMS570LC4357. In that I cannot make modification in R5-MPU-PMU tab.
And If I burn my code into the micro controller, It can not start working. It shows the following error while burning the code itself.
After this window comes, I can not do clicking start or pause icons.(See the above image). These icons are not enabled. So then I tried to burn any other working code. At that time following error occurred.
So to overcome this what I did is,
1. Holding the SYS_Reset button in the kit.
2. releasing that button when exactly the debugger do accessing TMS570LC4357.
After doing this my working code was loaded into the micro controller. And works fine only.
But my RTOS code is not even get loaded into micro controller and shows the same error sequence again and again.
Please anybody guide me where I fails.
Thanks in advance.
Regards,
Karthikeyan.K