This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Access to global variables in the external SDRAM



Hi,

I am working on the custom board based on TM4C1294+lwip1.4.1+freeRTOS+ccs5.5.x(Compiler ti v5.1.9).

but not sure I need to add "rtsv7M4_T_le_v4SPD16_eabi" in File Search Path of Linker.



I am developing a project from Stellaris(LM3S9B96) to Tiva C(TM4C1294).

My project requires EPI external 8MB SDRAM to store global variables, but the codes ,used to work in Stellaris, do not work in Tiva C.

To verify the 8MB SDRAM on the custom board, I executed the example of "sdram.c" and was able to write/read values from SDRAM.

In my project, All extern structs and variables are declared in one .h and their definitions are in one .c. The initialization of variables are done by a couple of init functions().

However, for test I just simplify codes using primitive data type instead of structs.

I have tried from 1 to 4

1.

#pragma DATA_SECTION(abab,".external");
extern int abab[20]; // ---------------> if I put extern here, compiler seems to ignore as a result I can not see the address on .map

2.
#pragma DATA_SECTION(abab,".external");
int abab[20]; // I can see the address on .map
or

3. 
extern int abab[20];
int abab[20]__attribute__ ((section (".external")));
4. 
extern int abab[20]__attribute__ ((section (".external")));
int abab[20];

//init values
memset((char *) abab ,0 ,sizeof(abab));

I can see the address "abab[]" in .map but everything I have tried on does not work as programing .bin. They just directly go to faultISR()

Even if I attempt to debug, it does not let me in since the program directly goes to faultISR().

I am not sure if this is due to compiler/linker problem or something wrong with my codes.

Thanks,

Jin

 

  • My guess is that the linker command file for the old project explicitly specifies where the ".external" section goes in memory, and the linker command file for the new project has no specification for ".external".  Please inspect the linker command file for the new project.  If I'm right, ".external" is not mentioned anywhere.  If that is the case, you need to add a specification for .external.  This wiki article will help you do that.

    Thanks and regards,

    -George

  • Hi George

    I  could see the address of ".external" in "linklnfo.xml" :

     <object_component id="oc-5ea">
             <name>.cinit..external.load</name>
             <load_address>0x2d28</load_address>
             <run_address>0x2d28</run_address>
             <size>0x8</size>
          </object_component>

             <cprec>
                <name>.external</name>
                <load_address>0x2d28</load_address>
                <load_size>0x8</load_size>
                <run_address>0x60000000</run_address>
                <run_size>0x50</run_size>
                <compression>zero_init</compression>
             </cprec>

    Also, I could see the below as well in ".map":

    __TI_cinit_table @ 00002d30 records: 3, size/record: 8, table size: 24
    	.data: load addr=00002cc8, load size=00000047 bytes, run addr=2002a5ac, run size=000000b0 bytes, compression=rle
    	.bss: load addr=00002d20, load size=00000008 bytes, run addr=20000000, run size=000265ac bytes, compression=zero_init
    	.external: load addr=00002d28, load size=00000008 bytes, run addr=60000000, run size=00000050 bytes, compression=zero_init
    
    

    Thanks,

    Jin

  • Please attach the entire map file to your next post.  You might need to add a ".txt" extension to it so it will be accepted.  

    Based on what I see here, there is a section named ".external", and it is located at address 0x60000000.  Given what you know about the system, does this address make sense?  Would accessing that address cause some kind of HW fault?

    Thanks and regards,

    -George

  • Hi George,

    Here is my .cmd :

    #define APP_BASE 0x00000000
    #define RAM_BASE 0x20000000
    #define SDRAM_BASE 0x60000000
    
    /* System memory map */
    
    MEMORY
    {
        /* Application stored in and executes from internal flash */
        FLASH (RX) : origin = APP_BASE, length = 0x00100000
        /* Application uses internal RAM for data */
        SRAM (RWX) : origin = 0x20000000, length = 0x00040000
        /* Application uses external RAM for large data arrays */
        SDRAM (RWX) : origin = SDRAM_BASE, length = 0x00800000
    }
    
    /* Section allocation in memory */
    
    SECTIONS
    {
        .intvecs:   > APP_BASE
        .text   :   > FLASH
        .const  :   > FLASH
        .cinit  :   > FLASH
        .pinit  :   > FLASH
        .init_array : > FLASH
    
        .vtable :   > RAM_BASE
        .data   :   > SRAM
        .bss    :   > SRAM
        .sysmem :   > SRAM
        .stack  :   > SRAM
        .external : > SDRAM
    }
    
    __STACK_TOP = __stack + 16384;

    As you see, the address of 8MB SDRAM starts at 0x60000000 and ends at 0x003FFFFF since (4Meg*16).

    Attached: linkinfo.xml and .map

    linkinfo_xml.txt

    map.txt

    As I ran the example of "sdram.c" to write/read values correctly. That's why I thought the external sdram on the custom board works fine.

    #define SDRAM_START_ADDRESS 0x00000000
    #define SDRAM_END_ADDRESS   0x003FFFFF
    g_pui16EPISdram = (uint16_t *)0x60000000;
    
    g_pui16EPISdram[SDRAM_START_ADDRESS] = 0xabcd;
        g_pui16EPISdram[SDRAM_START_ADDRESS + 1] = 0x1234;
        g_pui16EPISdram[SDRAM_END_ADDRESS - 1] = 0xdcba;
        g_pui16EPISdram[SDRAM_END_ADDRESS] = 0x4321;

    Regards,

    Jin

  • Here is one more thing to consider ... The boot routine _c_int00 runs straight from reset, before main is called.  The boot routine processes an initialization record which has the effect of writing the value 0 to the first 0x50 bytes of SDRAM (address 0x60000000).  I presume some SDRAM control registers (or something similar) must be configured prior to any write to SDRAM.  I'm not sure about the best way to configure these registers.  But that has to occur before the boot routine writes to SDRAM.

    Thanks and regards,

    -George

  • Hi George,

    Thank you for commenting on my question.

    I took a look at "Stellaris library" and found a couple of lib codes related with sdram.

    There is a initializing function( SDRAMInit() ) in /drivers/extram.c. It is quite similar with the example codes( sdram.c) in Tiva C except one thing below:

    bpool((void *)g_pusEPIMem, SDRAM_SIZE_BYTES);

    bpool() is defined in "bget.c" in Stellaris (third_party/bget).

    Is this needed to add on?


    Thanks,

    Jin

  • Your question is beyond my expertise.  I recommend you start a new thread in the TM4C device forum.  Or, if you prefer, I can move this thread into that forum.

    Thanks and regards,

    -George

  • HI George,

    Can you move this thread to TM4C forum?

    Thanks your support
    Jin
  • Hi George,

    I resolved the issue by activating EPI SDRAM before calling  _c_int00. Also

    bpool()

    has nothing to do with in this issue.

    Thank you for your support.

    Jin