Hello TI/QJ,
I noticed this in the bl_config.h file for the CAN bootloader:
//*****************************************************************************
//
// Selects the baud rate to be used for the UART.
//
// Depends on: UART_ENABLE_UPDATE
// Requires: None
// UART Baud Rates can be: 9600, 19200, 38400, 57600, 115200
//*****************************************************************************
#define UART_BAUDRATE 118200
#define UART sciREG1 /* Use UART port 1 for UART boot */
Should that be 115200? Guess it's a typo?
Is there a better place to post when this type of issue is found?
Thanks,
JohnW.