Hi,
I am working on a customized board with TM4C1290 with CCSV6.
when I use UARTCharPut(UART0_BASE, 'A');
I can see an output on the console, but if I used UARTprintf("\nConsole test!\n");
the program goes into faultISR
here is the code
#include<stdbool.h>
#include <stdint.h>
#include "inc/hw_memmap.h"
#include "inc/hw_types.h"
#include "driverlib/debug.h"
#include "driverlib/sysctl.h"
#include "driverlib/gpio.h"
#include "driverlib/sysctl.h"
#include "driverlib/uart.h"
#include "driverlib/pin_map.h"
#include "driverlib/adc.h"
#include "utils/uartstdio.h"
#include "driverlib/pwm.h"
uint32_t ui32SysClkFreq = 0;
void InitConsole(void)
{
SysCtlPeripheralEnable(SYSCTL_PERIPH_UART0);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);
GPIOPinConfigure(GPIO_PA0_U0RX);
GPIOPinConfigure(GPIO_PA1_U0TX);
GPIOPinTypeUART(GPIO_PORTA_BASE, GPIO_PIN_0 | GPIO_PIN_1);
UARTConfigSetExpClk(UART0_BASE, ui32SysClkFreq, 115200,(UART_CONFIG_WLEN_8 |
UART_CONFIG_STOP_ONE | UART_CONFIG_PAR_NONE));
UARTStdioConfig(0,115200,ui32SysClkFreq);
}
int main(void) {
ui32SysClkFreq = SysCtlClockFreqSet((SYSCTL_XTAL_25MHZ | SYSCTL_OSC_MAIN | SYSCTL_USE_PLL | SYSCTL_CFG_VCO_480), 120000000);
InitConsole();
UARTprintf("\nConsole test!\n");
//UARTCharPut(UART0_BASE, 'A');
while(1);
return 0;
}
Thanks.