Other Parts Discussed in Thread: HALCOGEN
I am trying to use the RM46 CRC module to calculate and verify CRC's for the linker generated CRC table. The problem that I am having is that the HalCoGen generaed crc driver (crc.h / crc.c) uses 64-bit words to generate the CRC (reference crcSignGen within crc.c).
If I try to apply a palign=8 to the .init_array section so it is 64-bit aligned and the size is aligned to 64-bits, the initialization for the global constructor has an issue since it uses the size of the .init_array section to call the list of constructors. The problem is that the palign=8 can pad the end of the .init_array with zeros or a defined fill, causing the run_pinit in the C++ startup to fail or try to run the addresses generated by the padding.
Any one run in to this same issue?
Link command file contains:
SECTIONS
{
.intvecs : {} align=8, crc_table(_vcmCrcTable, algorithm=TMS570_CRC64_ISO) > VECTORS
.text : {} align=8, crc_table(_vcmCrcTable, algorithm=TMS570_CRC64_ISO) > FLASH0
.const : {} align=8, crc_table(_vcmCrcTable, algorithm=TMS570_CRC64_ISO) > FLASH0
.cinit : {} align=8, crc_table(_vcmCrcTable, algorithm=TMS570_CRC64_ISO) > FLASH0
.init_array : {} align=8, crc_table(_vcmCrcTable, algorithm=TMS570_CRC64_ISO) > FLASH0
.TI.crctab {} > FLASH1
.bss : {} > RAM
.data : {} > RAM
.sysmem : {} > RAM
}
If the .init_array section is not aligned to 64-bit and the size is on a 64-bit boundary, that causes a problem with using the CRC module and DMA (64-bit transfers). If I force the alignment and size with the palign=8, the linker will pad zeros at the end of the .init_array section, thus causing problems with the run_pinit when it tries to use the section size to call all constructors (i.e. padded area causes the run_pinit to execute at address zero).
Here is run_init from the ti-cgt-arm_5.2.4/lib/src autoinit.h :
#pragma FUNC_ALWAYS_INLINE(run_pinit)
static __inline void run_pinit(void)
{
#ifdef __TI_EABI__
/*------------------------------------------------------------------------*/
/* Process Pinit table for ELF. */
/* The section is not NULL terminated, but can be accessed by pointers */
/* which point to the beginning and end of the section. */
/*------------------------------------------------------------------------*/
if (PINIT_BASE != PINIT_LIMIT)
{
int i = 0;
while (&(PINIT_BASE[i]) != PINIT_LIMIT)
PINIT_BASE[i++]();
}
#else
...
This initialization does not validate each of the constructor pointer in the table to be non-null prior to using?
Any help here would be greatly appreciated.
Thanks,
Don ...