Other Parts Discussed in Thread: TMS570LS0432, HALCOGEN
I can't find a reference guide to the N2HET instructions. The best I found was "TMS470R1x High-End Timer (HET) Reference Guide". Where is the document also covering the N2HET instructions?
I would like to have upto 10 PWM outputs with spread spectrum of 15kHz +-10% and I'm looking for an algorithm. It also needs to distribute PWM evenly to minimize current ripple in the output stages. Lets say all 10 PWM signals are 50% duty cycle, It would be stupid to have them all on at the same time because it would cause unnessesary current ripple in the output stage. I find this quite challenging. Is there algorithms for spreadspectrum PWM available? Any Ideas how to implement N2HET spread spectrum PWM?