Other Parts Discussed in Thread: UNIFLASH
Hi everyone!
I'm working with the RM57L Hercules Development Kit from TI.
It worked very good, but now i made a mistake to set the board to the sleep-Mode by using the command: "systemPowerDown(SYS_SLEEP_MODE);"
I flashed this code, and ran it while using break points and live debugging.
At the Moment the command was executed i lost the connection to the board.
Know there is the following problem, that i can't reconnect the board.
the error message is:
Error connecting to the target:
(Error -1170 @ 0x0)
Unable to access the DAP. Reset the device, and retry the operation.
If error persists, confirm configuration, power-cycle the board,
and/or try more reliable JTAG settings (e.g. lower TCLK).
(Emulation package 5.1.507.2)
I reset the board by using the "PORRST" and "RST" button on the board.
I also disconnected the main power supply, but that don't fixes the problem.
I want to get back the connection to the board to flash new programs.
Thank you very much!
Best regards,
Lukas Maul