This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

trying to send& recive using uart7 -tm4c1294xl

Hi i am using tm4c-1294xl 

i have managed to work according to the student guide lab10 and see input and outputs from the virtual com(uart0) but now i have decided to talk with another device using uart7 pins

for some reason i cant do this

attaching the code after changes from the uart echo example

help is super needed thanks :)

//*****************************************************************************
//
// uart_echo.c - Example for reading data from and writing data to the UART in
//               an interrupt driven fashion.
//
// Copyright (c) 2013-2014 Texas Instruments Incorporated.  All rights reserved.
// Software License Agreement
// 
// Texas Instruments (TI) is supplying this software for use solely and
// exclusively on TI's microcontroller products. The software is owned by
// TI and/or its suppliers, and is protected under applicable copyright
// laws. You may not combine this software with "viral" open-source
// software in order to form a larger program.
// 
// THIS SOFTWARE IS PROVIDED "AS IS" AND WITH ALL FAULTS.
// NO WARRANTIES, WHETHER EXPRESS, IMPLIED OR STATUTORY, INCLUDING, BUT
// NOT LIMITED TO, IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
// A PARTICULAR PURPOSE APPLY TO THIS SOFTWARE. TI SHALL NOT, UNDER ANY
// CIRCUMSTANCES, BE LIABLE FOR SPECIAL, INCIDENTAL, OR CONSEQUENTIAL
// DAMAGES, FOR ANY REASON WHATSOEVER.
// 
// This is part of revision 2.1.0.12573 of the EK-TM4C1294XL Firmware Package.
//
//*****************************************************************************

#include <stdint.h>
#include <stdbool.h>
#include "inc/hw_ints.h"
#include "inc/hw_memmap.h"
#include "driverlib/debug.h"
#include "driverlib/gpio.h"
#include "driverlib/interrupt.h"
#include "driverlib/pin_map.h"
#include "driverlib/rom.h"
#include "driverlib/rom_map.h"
#include "driverlib/sysctl.h"
#include "driverlib/uart.h"

//*****************************************************************************
//
//! \addtogroup example_list
//! <h1>UART Echo (uart_echo)</h1>
//!
//! This example application utilizes the UART to echo text.  The first UART
//! (connected to the USB debug virtual serial port on the evaluation board)
//! will be configured in 115,200 baud, 8-n-1 mode.  All characters received on
//! the UART are transmitted back to the UART.
//
//*****************************************************************************

//****************************************************************************
//
// System clock rate in Hz.
//
//****************************************************************************
uint32_t g_ui32SysClock;

//*****************************************************************************
//
// The error routine that is called if the driver library encounters an error.
//
//*****************************************************************************
#ifdef DEBUG
void
__error__(char *pcFilename, uint32_t ui32Line)
{
}
#endif

//*****************************************************************************
//
// The UART interrupt handler.
//
//*****************************************************************************
void
UARTIntHandler(void)
{
    uint32_t ui32Status;

    //
    // Get the interrrupt status.
    //
    ui32Status = ROM_UARTIntStatus(UART7_BASE, true);

    //
    // Clear the asserted interrupts.
    //
    ROM_UARTIntClear(UART7_BASE, ui32Status);

    //
    // Loop while there are characters in the receive FIFO.
    //
    while(ROM_UARTCharsAvail(UART7_BASE))
    {
        //
        // Read the next character from the UART and write it back to the UART.
        //
        ROM_UARTCharPutNonBlocking(UART7_BASE,
                                   ROM_UARTCharGetNonBlocking(UART7_BASE));

        //
        // Blink the LED to show a character transfer is occuring.
        //
        GPIOPinWrite(GPIO_PORTN_BASE, GPIO_PIN_0, GPIO_PIN_0);

        GPIOPinWrite(GPIO_PORTC_BASE, GPIO_PIN_4, GPIO_PIN_4);


        //
        // Delay for 1 millisecond.  Each SysCtlDelay is about 3 clocks.
        //
        SysCtlDelay(g_ui32SysClock / (1000 * 3));

        //
        // Turn off the LED
        //
        GPIOPinWrite(GPIO_PORTN_BASE, GPIO_PIN_0, 0);
    }
}

//*****************************************************************************
//
// Send a string to the UART.
//
//*****************************************************************************
void
UARTSend(const uint8_t *pui8Buffer, uint32_t ui32Count)
{
    //
    // Loop while there are more characters to send.
    //
    while(ui32Count--)
    {
        //
        // Write the next character to the UART.
        //
        ROM_UARTCharPutNonBlocking(UART7_BASE, *pui8Buffer++);
    }
}

//*****************************************************************************
//
// This example demonstrates how to send a string of data to the UART.
//
//*****************************************************************************
int
main(void)
{
    //
    // Set the clocking to run directly from the crystal at 120MHz.
    //
    g_ui32SysClock = MAP_SysCtlClockFreqSet((SYSCTL_XTAL_25MHZ |
                                             SYSCTL_OSC_MAIN |
                                             SYSCTL_USE_PLL |
                                             SYSCTL_CFG_VCO_480), 120000000);
    //
    // Enable the GPIO port that is used for the on-board LED.
    //
    ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPION);

    //
    // Enable the GPIO pins for the LED (PN0).
    //
    ROM_GPIOPinTypeGPIOOutput(GPIO_PORTN_BASE, GPIO_PIN_0);

    //
    // Enable the peripherals used by this example.
    //
    ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_UART7);
    ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);
    ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOC);

    //
    // Enable processor interrupts.
    //
    ROM_IntMasterEnable();

    //
    // Set GPIO A0 and A1 as UART pins.
    //
   // GPIOPinConfigure(GPIO_PA0_U0RX);
  //  GPIOPinConfigure(GPIO_PA1_U0TX);
  //  ROM_GPIOPinTypeUART(GPIO_PORTA_BASE, GPIO_PIN_0 | GPIO_PIN_1);


    //
    // Set GPIO A0 and A1 as UART pins.
    //
    GPIOPinConfigure(GPIO_PC4_U7RX);
    GPIOPinConfigure(GPIO_PC5_U7TX);
    //ROM_GPIOPinTypeUART(GPIO_PORTA_BASE, GPIO_PIN_0 | GPIO_PIN_1);
   // ROM_GPIOPinTypeUART(GPIO_PORTC_BASE, GPIO_PIN_0 | GPIO_PIN_1);
    ROM_GPIOPinTypeUART(GPIO_PORTC_BASE, GPIO_PIN_4 | GPIO_PIN_5);



    //
    // Configure the UART for 115,200, 8-N-1 operation.
    //
    ROM_UARTConfigSetExpClk(UART7_BASE, g_ui32SysClock, 115200,
                            (UART_CONFIG_WLEN_8 | UART_CONFIG_STOP_ONE |
                             UART_CONFIG_PAR_NONE));

    //
    // Enable the UART interrupt.
    //
    ROM_IntEnable(INT_UART7);
    ROM_UARTIntEnable(UART7_BASE, UART_INT_RX | UART_INT_RT);

    //
    // Prompt for text to be entered.
    //
    UARTSend((uint8_t *)"\033[2JEnter text: ", 16);

    //
    // Loop forever echoing data through the UART.
    //
    while(1)
    {
    	UARTSend((uint8_t *)"\033[2JEnter text: ", 16);

    }
}

  • Hello Idan

    The code looks correct. Did you check the UART RX and TX for transmission. What is the other device?

    Regards
    Amit
  • While help is, "super needed" the "need" for poster clarity - somehow - falls short.

    We're almost "never" told "How" poster's seek to connect and/or deploy their (changed) UART connections. There is NO ICDI present - to massage "normal" UART data into a form suitable for direct PC connection (via USB) - whenever the "default" UART is bypassed!

    Again & again this issue rises - yet such detail remains unaddressed...
  • Amit Ashara said:
    Hello Idan

    The code looks correct. Did you check the UART RX and TX for transmission. What is the other device?

    Regards
    Amit

    i am using a usb to uart dongle :

    CP2102 USB 2.0 to UART TTL 6PIN Module Serial Converter

    i am connecting the gnd,tx,rx pins only to the ti board

    then i am trying to open using putty a serial connection but without any success to see the messages that are being passed

  • Well it seems i found the probelm as it looks like the rx and tx pins are opposite!!
    meaning pc4 is tx and pc5 is rx - i thought i will try this and then it worked!!!

    Well i appricate the help and maybe its good idea to make some tutorial for all the connections
  • Wish to applaud you for:
    a) presenting the "solution" here - AND with sufficient "detail" so that many others may benefit! (i.e. clear id of the UART>-USB "dongle")
    b) identifying that "on-going" UART "pin change from past" GOTCHA - which (I believe) to be ineffectively high-lighted! Many have been so trapped - herd of turtles (motoring downhill, of course) would be faster to (properly) address...