Other Parts Discussed in Thread: LMFLASHPROGRAMMER
Hi, Everyone
I need your help
I wanna use ROM Boot Loader on DK-TM4C129X.
I was successful when I try to update after Program boot_demo_uart on Tivawware
with LMFLASHPROGRAMMER
and SPMS444B's BOOTCFG Register discription says
If the EN bit is set or the status doesn't match the specified polarity, the data at address
0x0000.0004 is read, and if the data at this address is 0xFFFF.FFFF, the ROM is mapped to
address 0x0000.0000 and execution continues out of the ROM Boot Loader.
But I erase Flash and try to update with ROM Boot Loder on LMFLASHPROGRAMMER.
But I got error.
I do not why.
I understand Tiva can upadate with ROM boot Loader after Flash wes erase
My undestanding is correct??
Berst Regards
Hiroyasu