Other Parts Discussed in Thread: MAX232
Hello everyone
I thank you if I can explain that I set the Tiva 129 for a program that captures data from the keyboard and send the USART 7. The example of "echo" Default configures the USART 0 and I could not set up to the output is the USART 7 main.c configure the pins, the GPIOs, and everything related to the use 7, but not working. Touch configure some additional .h file ?, or otherwise should be performed.
I've also tried with the qs example that brings that same function "echo" but neither works.
I think the problem is that no catch keyboard is performed.
Thank you very much for your attention.
I thank you I work with ideas, or any other alternative or program that realize this function.