Other Parts Discussed in Thread: HALCOGEN
In TMS570LS31x HETGCR register bit 24 (HET PIN ENA) always reads zero even if the bit is set to 1. In TRM the bit is defined as R/W-1 , which means that the value after reset should be 1. Is there a mistake in the TRM?