Other Parts Discussed in Thread: MSP-EXP430FR5969
Hi,
I see that new booster pack Kentec QVGA S1 has been changed from 8-bit parallel interface to SPI interface. So I am attaching the driver for new interface (SPI Interface) and I hope that it will be helpful for others.
Best Regards,
Sattar Malokani
//*****************************************************************************
//
// Kentec320x240x16_ssd2119_SPI.c - Display driver for the Kentec
// BOOSTXL-K350QVG-S1 TFT display with an SSD2119
// controller. This version assumes an SPI interface
// between the micro and display.
//
//*****************************************************************************
//*****************************************************************************
//
//! \addtogroup display_api
//! @{
//
//*****************************************************************************
#include <stdint.h>
#include <stdbool.h>
#include "inc/hw_gpio.h"
#include "inc/hw_ints.h"
#include "inc/hw_memmap.h"
#include "inc/hw_types.h"
#include "driverlib/ssi.h"
#include "driverlib/gpio.h"
#include "driverlib/interrupt.h"
#include "driverlib/sysctl.h"
#include "driverlib/timer.h"
#include "driverlib/rom.h"
#include "driverlib/pin_map.h"
#include "grlib/grlib.h"
#include "drivers/Kentec320x240x16_SSD2119_SPI.h"
//*****************************************************************************
//
// This driver operates in four different screen orientations. They are:
//
// * Portrait - The screen is taller than it is wide, and the flex connector is
// on the left of the display. This is selected by defining
// PORTRAIT.
//
// * Landscape - The screen is wider than it is tall, and the flex connector is
// on the bottom of the display. This is selected by defining
// LANDSCAPE.
//
// * Portrait flip - The screen is taller than it is wide, and the flex
// connector is on the right of the display. This is
// selected by defining PORTRAIT_FLIP.
//
// * Landscape flip - The screen is wider than it is tall, and the flex
// connector is on the top of the display. This is
// selected by defining LANDSCAPE_FLIP.
//
// These can also be imagined in terms of screen rotation; if portrait mode is
// 0 degrees of screen rotation, landscape is 90 degrees of counter-clockwise
// rotation, portrait flip is 180 degrees of rotation, and landscape flip is
// 270 degress of counter-clockwise rotation.
//
// If no screen orientation is selected, "landscape flip" mode will be used.
//
//*****************************************************************************
#if ! defined(PORTRAIT) && ! defined(PORTRAIT_FLIP) && \
! defined(LANDSCAPE) && ! defined(LANDSCAPE_FLIP)
#define LANDSCAPE
//#define PORTRAIT_FLIP
#endif
//*****************************************************************************
//
// Various definitions controlling coordinate space mapping and drawing
// direction in the four supported orientations.
//
//*****************************************************************************
#ifdef PORTRAIT
#define HORIZ_DIRECTION 0x28
#define VERT_DIRECTION 0x20
#define MAPPED_X(x, y) (319 - (y))
#define MAPPED_Y(x, y) (x)
#endif
#ifdef LANDSCAPE
#define HORIZ_DIRECTION 0x00
#define VERT_DIRECTION 0x08
#define MAPPED_X(x, y) (319 - (x))
#define MAPPED_Y(x, y) (239 - (y))
#endif
#ifdef PORTRAIT_FLIP
#define HORIZ_DIRECTION 0x18
#define VERT_DIRECTION 0x10
#define MAPPED_X(x, y) (y)
#define MAPPED_Y(x, y) (239 - (x))
#endif
#ifdef LANDSCAPE_FLIP
#define HORIZ_DIRECTION 0x30
#define VERT_DIRECTION 0x38
#define MAPPED_X(x, y) (x)
#define MAPPED_Y(x, y) (y)
#endif
//#define SPI3 //9-bit 3-wire SPI (SSI2) mode (SCLK, SDA, SCS)
// Default setting for the BOOSTXL-K350QVG-S1
// Need to remove the "R10" (connect the "PB7/SSI2Tx" to "PD1/AIN6_TOUCH_XP") on Launchpad
#define SPI4 //8-bit 4-wire SPI (SSI2) mode (SCLK, SDA, SCS, SDC)
// Need to remove the "R10" (connect the "PB7/SSI2Tx" to "PD1/AIN6_TOUCH_XP") on Launchpad
// Need to move the "R2" to "R3" position,
// and move "R8" to "R9" position on the BOOSTXL-K350QVG-S1
//*****************************************************************************
//
// Defines for the pins that are used to communicate with the SSD2119.
//
//*****************************************************************************
#define LCD_CS_PERIPH SYSCTL_PERIPH_GPIOA
#define LCD_CS_BASE GPIO_PORTA_BASE
#define LCD_CS_PIN GPIO_PIN_4
#define LCD_DC_PERIPH SYSCTL_PERIPH_GPIOA
#define LCD_DC_BASE GPIO_PORTA_BASE
#define LCD_DC_PIN GPIO_PIN_5
#define LCD_RST_PERIPH SYSCTL_PERIPH_GPIOD
#define LCD_RST_BASE GPIO_PORTD_BASE
#define LCD_RST_PIN GPIO_PIN_7
#define LCD_LED_PERIPH SYSCTL_PERIPH_GPIOF
#define LCD_LED_BASE GPIO_PORTF_BASE
#define LCD_LED_PIN GPIO_PIN_2
//*****************************************************************************
//
// The dimensions of the LCD panel.
//
//*****************************************************************************
#define LCD_VERTICAL_MAX 240
#define LCD_HORIZONTAL_MAX 320
#define SSD2119_ENTRY_MODE_REG 0x11
#define SSD2119_RAM_DATA_REG 0x22
#define SSD2119_V_RAM_POS_REG 0x44
#define SSD2119_H_RAM_START_REG 0x45
#define SSD2119_H_RAM_END_REG 0x46
#define SSD2119_X_RAM_ADDR_REG 0x4E
#define SSD2119_Y_RAM_ADDR_REG 0x4F
#define ENTRY_MODE_DEFAULT 0x6830
#define MAKE_ENTRY_MODE(x) ((ENTRY_MODE_DEFAULT & 0xFF00) | (x))
//*****************************************************************************
//
// Translates a 24-bit RGB color to a display driver-specific color.
//
// \param c is the 24-bit RGB color. The least-significant byte is the blue
// channel, the next byte is the green channel, and the third byte is the red
// channel.
//
// This macro translates a 24-bit RGB color into a value that can be written
// into the display's frame buffer in order to reproduce that color, or the
// closest possible approximation of that color.
//
// \return Returns the display-driver specific color.
//
//*****************************************************************************
#define DPYCOLORTRANSLATE(c) ((((c) & 0x00f80000) >> 8) | \
(((c) & 0x0000fc00) >> 5) | \
(((c) & 0x000000f8) >> 3))
//*****************************************************************************
//
// Macro used to set the LCD data bus in preparation for writing a byte to the
// device.
//
//*****************************************************************************
uint16_t pui16Data[2];
#ifdef SPI3
//*****************************************************************************
// Writes a data word to the SSD2119. This function implements the 3-wire SPI
// interface to the LCD display.
//*****************************************************************************
static void
WriteDataSPI(unsigned short usData)
{
pui16Data[0] = 0x100 | (usData >> 8);// set the most significant byte of the data.
pui16Data[1] = 0x100 | usData;// set the least significant byte of the data.
HWREG(LCD_CS_BASE + GPIO_O_DATA + (LCD_CS_PIN << 2)) = 0;//CS="0"
SSIDataPut(SSI2_BASE, pui16Data[0]);
SSIDataPut(SSI2_BASE, pui16Data[1]);
while(SSIBusy(SSI2_BASE)){ } // Wait until SSI0 is done transferring all the data in the transmit FIFO.
HWREG(LCD_CS_BASE + GPIO_O_DATA + (LCD_CS_PIN << 2)) = LCD_CS_PIN;
}
//*****************************************************************************
// Writes register word to the SSD2119. This function implements the 3-wire SPI
// interface to the LCD display.
//*****************************************************************************
static void
WriteCommandSPI(unsigned short usData)
{
pui16Data[0] = 0;// set the most significant byte of the data.
pui16Data[1] = 0xFF & usData;// set the least significant byte of the data.
HWREG(LCD_CS_BASE + GPIO_O_DATA + (LCD_CS_PIN << 2)) = 0;//CS="0"
SSIDataPut(SSI2_BASE, pui16Data[0]);
SSIDataPut(SSI2_BASE, pui16Data[1]);
while(SSIBusy(SSI2_BASE)){ } // Wait until SSI0 is done transferring all the data in the transmit FIFO.
HWREG(LCD_CS_BASE + GPIO_O_DATA + (LCD_CS_PIN << 2)) = LCD_CS_PIN;
}
#endif
#ifdef SPI4
//*****************************************************************************
// Writes a data word to the SSD2119. This function implements the 4-wire SPI
// interface to the LCD display.
//*****************************************************************************
static void
WriteDataSPI(unsigned short usData)
{
pui16Data[0] = (usData >> 8);// Write the most significant byte of the data to the bus.
pui16Data[1] = usData;// Write the least significant byte of the data to the bus.
HWREG(LCD_DC_BASE + GPIO_O_DATA + (LCD_DC_PIN << 2)) = LCD_DC_PIN;//DC="1"
HWREG(LCD_CS_BASE + GPIO_O_DATA + (LCD_CS_PIN << 2)) = 0;//CS="0"
SSIDataPut(SSI2_BASE, pui16Data[0]);
SSIDataPut(SSI2_BASE, pui16Data[1]);
while(SSIBusy(SSI2_BASE)){ } // Wait until SSI0 is done transferring all the data in the transmit FIFO.
HWREG(LCD_CS_BASE + GPIO_O_DATA + (LCD_CS_PIN << 2)) = LCD_CS_PIN;
}
//*****************************************************************************
// Writes register word to the SSD2119. This function implements the 3-wire SPI
// interface to the LCD display.
//*****************************************************************************
static void
WriteCommandSPI(unsigned short usData)
{
pui16Data[0] = 0;// Write the most significant byte of the data to the bus.
pui16Data[1] = usData;// Write the least significant byte of the data to the bus.
HWREG(LCD_DC_BASE + GPIO_O_DATA + (LCD_DC_PIN << 2)) = 0;//DC="0"
HWREG(LCD_CS_BASE + GPIO_O_DATA + (LCD_CS_PIN << 2)) = 0;//CS="0"
SSIDataPut(SSI2_BASE, pui16Data[0]);
SSIDataPut(SSI2_BASE, pui16Data[1]);
while(SSIBusy(SSI2_BASE)){ } // Wait until SSI0 is done transferring all the data in the transmit FIFO.
HWREG(LCD_CS_BASE + GPIO_O_DATA + (LCD_CS_PIN << 2)) = LCD_CS_PIN;
}
#endif
//*****************************************************************************
// Initializes the LCD interface.
// Enable the SSI2 for LCD data/register transfer.
// Set the LCD_CS_PIN, LCD_DC_PIN, LCD_RST_PIN.
//*****************************************************************************
static void
LCD_PORT_Init(void)
{
uint32_t pui32DataRx[3];
// The SSI2 peripheral must be enabled for use.
SysCtlPeripheralEnable(SYSCTL_PERIPH_SSI2);
// For this example SSI2 is used with PortB[7:4]. The actual port and pins
// used may be different on your part, consult the data sheet for more
// information. GPIO port B needs to be enabled so these pins can be used.
// TODO: change this to whichever GPIO port you are using.
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOB);
// Enable the PortA[5:4] for the LCD_SCS, LCD_SDC
// Enable the PortD[7] for LCD_RST
// Enable the PortF[2] for LED backlight
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOD);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOF);
// Change PD7 into GPIO output.
HWREG(GPIO_PORTD_BASE + GPIO_O_LOCK) |= GPIO_LOCK_KEY;
HWREG(GPIO_PORTD_BASE + GPIO_O_CR) |= 0x80;
HWREG(GPIO_PORTD_BASE + GPIO_O_AFSEL) &= 0x7f;
GPIOPinTypeGPIOOutput(LCD_RST_BASE, LCD_RST_PIN);
GPIOPinTypeGPIOOutput(LCD_CS_BASE, LCD_CS_PIN);
GPIOPinTypeGPIOOutput(LCD_DC_BASE, LCD_DC_PIN);
GPIOPinTypeGPIOOutput(LCD_LED_BASE, LCD_LED_PIN);
//GPIOPadConfigSet(LCD_LED_BASE, LCD_LED_PIN, GPIO_STRENGTH_8MA, GPIO_PIN_TYPE_STD);
// Configure the pin muxing for SSI2 functions on port B4, B5, B6, and B7.
// This step is not necessary if your part does not support pin muxing.
// TODO: change this to select the port/pin you are using.
GPIOPinConfigure(GPIO_PB4_SSI2CLK);
GPIOPinConfigure(GPIO_PB5_SSI2FSS);
GPIOPinConfigure(GPIO_PB6_SSI2RX);
GPIOPinConfigure(GPIO_PB7_SSI2TX);
// Configure the GPIO settings for the SSI pins. This function also gives
// control of these pins to the SSI hardware. Consult the data sheet to
// see which functions are allocated per pin.
// The pins are assigned as follows:
// PB7 - SSI2Tx
// PB6 - SSI2Rx
// PB5 - SSI2Fss
// PB4 - SSI2CLK
// TODO: change this to select the port/pin you are using.
GPIOPinTypeSSI(GPIO_PORTB_BASE, GPIO_PIN_7 | GPIO_PIN_6 | GPIO_PIN_5 | GPIO_PIN_4);
GPIOPadConfigSet(GPIO_PORTB_BASE, GPIO_PIN_7, GPIO_STRENGTH_8MA, GPIO_PIN_TYPE_STD);
// Configure and enable the SSI port for SPI master mode. Use SSI0,
// system clock supply, idle clock level low and active low clock in
// freescale SPI mode, master mode, 1MHz SSI frequency, and 8-bit data.
// For SPI mode, you can set the polarity of the SSI clock when the SSI
// unit is idle. You can also configure what clock edge you want to
// capture data on. Please reference the datasheet for more information on
// the different SPI modes.
#ifdef SPI3
SSIConfigSetExpClk(SSI2_BASE, SysCtlClockGet(), SSI_FRF_MOTO_MODE_0, SSI_MODE_MASTER, 20000000, 9);
#endif
#ifdef SPI4
SSIConfigSetExpClk(SSI2_BASE, SysCtlClockGet(), SSI_FRF_MOTO_MODE_0, SSI_MODE_MASTER, 20000000, 8);
#endif
// Enable the SSI2 module.
SSIEnable(SSI2_BASE);
// Read any residual data from the SSI port. This makes sure the receive
// FIFOs are empty, so we don't read any unwanted junk. This is done here
// because the SPI SSI mode is full-duplex, which allows you to send and
// receive at the same time. The SSIDataGetNonBlocking function returns
// "true" when data was returned, and "false" when no data was returned.
// The "non-blocking" function checks if there is any data in the receive
// FIFO and does not "hang" if there isn't.
while(SSIDataGetNonBlocking(SSI2_BASE, &pui32DataRx[0])) { }
}
void LED_backlight_ON(void)
{
HWREG(LCD_LED_BASE + GPIO_O_DATA + (LCD_LED_PIN << 2)) = LCD_LED_PIN;
}
void LED_backlight_OFF(void)
{
HWREG(LCD_LED_BASE + GPIO_O_DATA + (LCD_LED_PIN << 2)) = 0;
}
//*****************************************************************************
//
//! Initializes the display driver.
//!
//! This function initializes the SSD2119 display controller on the panel,
//! preparing it to display data.
//!
//! \return None.
//
//*****************************************************************************
void
Kentec320x240x16_SSD2119Init(void)
{
unsigned int ulClockMS, ulCount;
// Get the current processor clock frequency.
ulClockMS = SysCtlClockGet() / (3 * 1000);
// Initializes the LCD port
LCD_PORT_Init();
// Reset the LCD
HWREG(LCD_RST_BASE + GPIO_O_DATA + (LCD_RST_PIN << 2)) = 0;//RST="0"
SysCtlDelay(10 * ulClockMS);
HWREG(LCD_RST_BASE + GPIO_O_DATA + (LCD_RST_PIN << 2)) = LCD_RST_PIN;//RST="1"
SysCtlDelay(20 * ulClockMS);
// Enter sleep mode (if we are not already there).
WriteCommandSPI(0x10);//SLEEP_MODE_REG
WriteDataSPI(0x0001);
//
// Set initial power parameters.
//
WriteCommandSPI(0x1E);//SSD2119_PWR_CTRL_5_REG
WriteDataSPI(0x00BA);
WriteCommandSPI(0x28);//SSD2119_VCOM_OTP_1_REG
WriteDataSPI(0x0006);
//
// Start the oscillator.
//
WriteCommandSPI(0x00);
WriteDataSPI(0x0001);
//
// Set pixel format and basic display orientation (scanning direction).
//
WriteCommandSPI(0x01);
WriteDataSPI(0x30EF);
WriteCommandSPI(0x02);
WriteDataSPI(0x0600);
//
// Exit sleep mode.
//
WriteCommandSPI(0x10);//SSD2119_SLEEP_MODE_REG
WriteDataSPI(0x0000);
//
// Delay 30mS
//
SysCtlDelay(30 * ulClockMS);
//
// Configure pixel color format and MCU interface parameters.
//
WriteCommandSPI(SSD2119_ENTRY_MODE_REG);
WriteDataSPI(ENTRY_MODE_DEFAULT);
//
// Enable the display.
//
WriteCommandSPI(0x07);
WriteDataSPI(0x0033);
//
// Set VCIX2 voltage to 6.1V.
//
WriteCommandSPI(0x0C);//SSD2119_PWR_CTRL_2_REG
WriteDataSPI(0x0005);
//
// Configure gamma correction.
//
WriteCommandSPI(0x30); WriteDataSPI(0x0000);//SSD2119_GAMMA_CTRL_1
WriteCommandSPI(0x31); WriteDataSPI(0x0400);//SSD2119_GAMMA_CTRL_2
WriteCommandSPI(0x32); WriteDataSPI(0x0106);//SSD2119_GAMMA_CTRL_3
WriteCommandSPI(0x33); WriteDataSPI(0x0700);//SSD2119_GAMMA_CTRL_4
WriteCommandSPI(0x34); WriteDataSPI(0x0002);//SSD2119_GAMMA_CTRL_5
WriteCommandSPI(0x35); WriteDataSPI(0x0702);//SSD2119_GAMMA_CTRL_6
WriteCommandSPI(0x36); WriteDataSPI(0x0707);//SSD2119_GAMMA_CTRL_7
WriteCommandSPI(0x37); WriteDataSPI(0x0203);//SSD2119_GAMMA_CTRL_8
WriteCommandSPI(0x3A); WriteDataSPI(0x1400);//SSD2119_GAMMA_CTRL_9
WriteCommandSPI(0x3B); WriteDataSPI(0x0F03);//SSD2119_GAMMA_CTRL_10
//
// Configure Vlcd63 and VCOMl.
//
WriteCommandSPI(0x0D);//SSD2119_PWR_CTRL_3_REG
WriteDataSPI(0x0007);
WriteCommandSPI(0x0E);//SSD2119_PWR_CTRL_4_REG
WriteDataSPI(0x3100);
//
// Set the display size and ensure that the GRAM window is set to allow
// access to the full display buffer.
//
WriteCommandSPI(SSD2119_V_RAM_POS_REG);
WriteDataSPI((LCD_VERTICAL_MAX-1) << 8);
WriteCommandSPI(SSD2119_H_RAM_START_REG);
WriteDataSPI(0x0000);
WriteCommandSPI(SSD2119_H_RAM_END_REG);
WriteDataSPI(LCD_HORIZONTAL_MAX-1);
WriteCommandSPI(SSD2119_X_RAM_ADDR_REG);
WriteDataSPI(0x00);
WriteCommandSPI(SSD2119_Y_RAM_ADDR_REG);
WriteDataSPI(0x00);
// Clear the contents of the display buffer.
WriteCommandSPI(SSD2119_RAM_DATA_REG);
for(ulCount = 0; ulCount < (320 * 240); ulCount++)
{
WriteDataSPI(0x0000);
}
LED_backlight_ON();
}
//*****************************************************************************
//
//! Draws a pixel on the screen.
//!
//! \param pvDisplayData is a pointer to the driver-specific data for this
//! display driver.
//! \param lX is the X coordinate of the pixel.
//! \param lY is the Y coordinate of the pixel.
//! \param ulValue is the color of the pixel.
//!
//! This function sets the given pixel to a particular color. The coordinates
//! of the pixel are assumed to be within the extents of the display.
//!
//! \return None.
//
//*****************************************************************************
static void
Kentec320x240x16_SSD2119PixelDraw(void *pvDisplayData, int lX, int lY,
unsigned int ulValue)
{
//
// Set the X address of the display cursor.
//
WriteCommandSPI(SSD2119_X_RAM_ADDR_REG);
WriteDataSPI(MAPPED_X(lX, lY));
//
// Set the Y address of the display cursor.
//
WriteCommandSPI(SSD2119_Y_RAM_ADDR_REG);
WriteDataSPI(MAPPED_Y(lX, lY));
//
// Write the pixel value.
//
WriteCommandSPI(SSD2119_RAM_DATA_REG);
WriteDataSPI(ulValue);
}
//*****************************************************************************
//
//! Draws a horizontal sequence of pixels on the screen.
//!
//! \param pvDisplayData is a pointer to the driver-specific data for this
//! display driver.
//! \param lX is the X coordinate of the first pixel.
//! \param lY is the Y coordinate of the first pixel.
//! \param lX0 is sub-pixel offset within the pixel data, which is valid for 1
//! or 4 bit per pixel formats.
//! \param lCount is the number of pixels to draw.
//! \param lBPP is the number of bits per pixel; must be 1, 4, or 8.
//! \param pucData is a pointer to the pixel data. For 1 and 4 bit per pixel
//! formats, the most significant bit(s) represent the left-most pixel.
//! \param pucPalette is a pointer to the palette used to draw the pixels.
//!
//! This function draws a horizontal sequence of pixels on the screen, using
//! the supplied palette. For 1 bit per pixel format, the palette contains
//! pre-translated colors; for 4 and 8 bit per pixel formats, the palette
//! contains 24-bit RGB values that must be translated before being written to
//! the display.
//!
//! \return None.
//
//*****************************************************************************
static void
Kentec320x240x16_SSD2119PixelDrawMultiple(void *pvDisplayData, int lX,
int lY, int lX0, int lCount,
int lBPP,
const unsigned char *pucData,
const unsigned char *pucPalette)
{
unsigned int ulByte;
//
// Set the cursor increment to left to right, followed by top to bottom.
//
WriteCommandSPI(SSD2119_ENTRY_MODE_REG);
WriteDataSPI(MAKE_ENTRY_MODE(HORIZ_DIRECTION));
//
// Set the starting X address of the display cursor.
//
WriteCommandSPI(SSD2119_X_RAM_ADDR_REG);
WriteDataSPI(MAPPED_X(lX, lY));
//
// Set the Y address of the display cursor.
//
WriteCommandSPI(SSD2119_Y_RAM_ADDR_REG);
WriteDataSPI(MAPPED_Y(lX, lY));
//
// Write the data RAM write command.
//
WriteCommandSPI(SSD2119_RAM_DATA_REG);
//
// Determine how to interpret the pixel data based on the number of bits
// per pixel.
//
switch(lBPP)
{
//
// The pixel data is in 1 bit per pixel format.
//
case 1:
{
//
// Loop while there are more pixels to draw.
//
while(lCount)
{
//
// Get the next byte of image data.
//
ulByte = *pucData++;
//
// Loop through the pixels in this byte of image data.
//
for(; (lX0 < 8) && lCount; lX0++, lCount--)
{
//
// Draw this pixel in the appropriate color.
//
WriteDataSPI(((unsigned int *)pucPalette)[(ulByte >>
(7 - lX0)) & 1]);
}
//
// Start at the beginning of the next byte of image data.
//
lX0 = 0;
}
//
// The image data has been drawn.
//
break;
}
//
// The pixel data is in 4 bit per pixel format.
//
case 4:
{
//
// Loop while there are more pixels to draw. "Duff's device" is
// used to jump into the middle of the loop if the first nibble of
// the pixel data should not be used. Duff's device makes use of
// the fact that a case statement is legal anywhere within a
// sub-block of a switch statement. See
// http://en.wikipedia.org/wiki/Duff's_device for detailed
// information about Duff's device.
//
switch(lX0 & 1)
{
case 0:
while(lCount)
{
//
// Get the upper nibble of the next byte of pixel data
// and extract the corresponding entry from the
// palette.
//
ulByte = (*pucData >> 4) * 3;
ulByte = (*(unsigned int *)(pucPalette + ulByte) &
0x00ffffff);
//
// Translate this palette entry and write it to the
// screen.
//
WriteDataSPI(DPYCOLORTRANSLATE(ulByte));
//
// Decrement the count of pixels to draw.
//
lCount--;
//
// See if there is another pixel to draw.
//
if(lCount)
{
case 1:
//
// Get the lower nibble of the next byte of pixel
// data and extract the corresponding entry from
// the palette.
//
ulByte = (*pucData++ & 15) * 3;
ulByte = (*(unsigned int *)(pucPalette + ulByte) &
0x00ffffff);
//
// Translate this palette entry and write it to the
// screen.
//
WriteDataSPI(DPYCOLORTRANSLATE(ulByte));
//
// Decrement the count of pixels to draw.
//
lCount--;
}
}
}
//
// The image data has been drawn.
//
break;
}
//
// The pixel data is in 8 bit per pixel format.
//
case 8:
{
//
// Loop while there are more pixels to draw.
//
while(lCount--)
{
//
// Get the next byte of pixel data and extract the
// corresponding entry from the palette.
//
ulByte = *pucData++ * 3;
ulByte = *(unsigned int *)(pucPalette + ulByte) & 0x00ffffff;
//
// Translate this palette entry and write it to the screen.
//
WriteDataSPI(DPYCOLORTRANSLATE(ulByte));
}
//
// The image data has been drawn.
//
break;
}
//
// We are being passed data in the display's native format. Merely
// write it directly to the display. This is a special case which is
// not used by the graphics library but which is helpful to
// applications which may want to handle, for example, JPEG images.
//
case 16:
{
unsigned short usByte;
//
// Loop while there are more pixels to draw.
//
while(lCount--)
{
//
// Get the next byte of pixel data and extract the
// corresponding entry from the palette.
//
usByte = *((unsigned short *)pucData);
pucData += 2;
//
// Translate this palette entry and write it to the screen.
//
WriteDataSPI(usByte);
}
}
}
}
//*****************************************************************************
//
//! Draws a horizontal line.
//!
//! \param pvDisplayData is a pointer to the driver-specific data for this
//! display driver.
//! \param lX1 is the X coordinate of the start of the line.
//! \param lX2 is the X coordinate of the end of the line.
//! \param lY is the Y coordinate of the line.
//! \param ulValue is the color of the line.
//!
//! This function draws a horizontal line on the display. The coordinates of
//! the line are assumed to be within the extents of the display.
//!
//! \return None.
//
//*****************************************************************************
static void
Kentec320x240x16_SSD2119LineDrawH(void *pvDisplayData, int lX1, int lX2,
int lY, unsigned int ulValue)
{
//
// Set the cursor increment to left to right, followed by top to bottom.
//
WriteCommandSPI(SSD2119_ENTRY_MODE_REG);
WriteDataSPI(MAKE_ENTRY_MODE(HORIZ_DIRECTION));
//
// Set the starting X address of the display cursor.
//
WriteCommandSPI(SSD2119_X_RAM_ADDR_REG);
WriteDataSPI(MAPPED_X(lX1, lY));
//
// Set the Y address of the display cursor.
//
WriteCommandSPI(SSD2119_Y_RAM_ADDR_REG);
WriteDataSPI(MAPPED_Y(lX1, lY));
//
// Write the data RAM write command.
//
WriteCommandSPI(SSD2119_RAM_DATA_REG);
//
// Loop through the pixels of this horizontal line.
//
while(lX1++ <= lX2)
{
//
// Write the pixel value.
//
WriteDataSPI(ulValue);
}
}
//*****************************************************************************
//
//! Draws a vertical line.
//!
//! \param pvDisplayData is a pointer to the driver-specific data for this
//! display driver.
//! \param lX is the X coordinate of the line.
//! \param lY1 is the Y coordinate of the start of the line.
//! \param lY2 is the Y coordinate of the end of the line.
//! \param ulValue is the color of the line.
//!
//! This function draws a vertical line on the display. The coordinates of the
//! line are assumed to be within the extents of the display.
//!
//! \return None.
//
//*****************************************************************************
static void
Kentec320x240x16_SSD2119LineDrawV(void *pvDisplayData, int lX, int lY1,
int lY2, unsigned int ulValue)
{
//
// Set the cursor increment to top to bottom, followed by left to right.
//
WriteCommandSPI(SSD2119_ENTRY_MODE_REG);
WriteDataSPI(MAKE_ENTRY_MODE(VERT_DIRECTION));
//
// Set the X address of the display cursor.
//
WriteCommandSPI(SSD2119_X_RAM_ADDR_REG);
WriteDataSPI(MAPPED_X(lX, lY1));
//
// Set the starting Y address of the display cursor.
//
WriteCommandSPI(SSD2119_Y_RAM_ADDR_REG);
WriteDataSPI(MAPPED_Y(lX, lY1));
//
// Write the data RAM write command.
//
WriteCommandSPI(SSD2119_RAM_DATA_REG);
//
// Loop through the pixels of this vertical line.
//
while(lY1++ <= lY2)
{
//
// Write the pixel value.
//
WriteDataSPI(ulValue);
}
}
//*****************************************************************************
//
//! Fills a rectangle.
//!
//! \param pvDisplayData is a pointer to the driver-specific data for this
//! display driver.
//! \param pRect is a pointer to the structure describing the rectangle.
//! \param ulValue is the color of the rectangle.
//!
//! This function fills a rectangle on the display. The coordinates of the
//! rectangle are assumed to be within the extents of the display, and the
//! rectangle specification is fully inclusive (in other words, both sXMin and
//! sXMax are drawn, along with sYMin and sYMax).
//!
//! \return None.
//
//*****************************************************************************
static void
Kentec320x240x16_SSD2119RectFill(void *pvDisplayData, const tRectangle *pRect,
unsigned int ulValue)
{
int lCount;
//
// Write the Y extents of the rectangle.
//
WriteCommandSPI(SSD2119_ENTRY_MODE_REG);
WriteDataSPI(MAKE_ENTRY_MODE(HORIZ_DIRECTION));
//
// Write the X extents of the rectangle.
//
WriteCommandSPI(SSD2119_H_RAM_START_REG);
#if (defined PORTRAIT) || (defined LANDSCAPE)
WriteDataSPI(MAPPED_X(pRect->i16XMax, pRect->i16YMax));
#else
WriteDataSPI(MAPPED_X(pRect->i16XMin, pRect->i16YMin));
#endif
WriteCommandSPI(SSD2119_H_RAM_END_REG);
#if (defined PORTRAIT) || (defined LANDSCAPE)
WriteDataSPI(MAPPED_X(pRect->i16XMin, pRect->i16YMin));
#else
WriteDataSPI(MAPPED_X(pRect->i16XMax, pRect->i16YMax));
#endif
//
// Write the Y extents of the rectangle
//
WriteCommandSPI(SSD2119_V_RAM_POS_REG);
#if (defined LANDSCAPE_FLIP) || (defined PORTRAIT)
WriteDataSPI(MAPPED_Y(pRect->i16XMin, pRect->i16YMin) |
(MAPPED_Y(pRect->i16XMax, pRect->i16YMax) << 8));
#else
WriteDataSPI(MAPPED_Y(pRect->i16XMax, pRect->i16YMax) |
(MAPPED_Y(pRect->i16XMin, pRect->i16YMin) << 8));
#endif
//
// Set the display cursor to the upper left of the rectangle (in application
// coordinate space).
//
WriteCommandSPI(SSD2119_X_RAM_ADDR_REG);
WriteDataSPI(MAPPED_X(pRect->i16XMin, pRect->i16YMin));
WriteCommandSPI(SSD2119_Y_RAM_ADDR_REG);
WriteDataSPI(MAPPED_Y(pRect->i16XMin, pRect->i16YMin));
//
// Tell the controller we are about to write data into its RAM.
//
WriteCommandSPI(SSD2119_RAM_DATA_REG);
//
// Loop through the pixels of this filled rectangle.
//
for(lCount = ((pRect->i16XMax - pRect->i16XMin + 1) *
(pRect->i16YMax - pRect->i16YMin + 1)); lCount >= 0; lCount--)
{
//
// Write the pixel value.
//
WriteDataSPI(ulValue);
}
//
// Reset the X extents to the entire screen.
//
WriteCommandSPI(SSD2119_H_RAM_START_REG);
WriteDataSPI(0x0000);
WriteCommandSPI(SSD2119_H_RAM_END_REG);
WriteDataSPI(0x013F);
//
// Reset the Y extent to the full screen
//
WriteCommandSPI(SSD2119_V_RAM_POS_REG);
WriteDataSPI(0xEF00);
}
//*****************************************************************************
//
//! Translates a 24-bit RGB color to a display driver-specific color.
//!
//! \param pvDisplayData is a pointer to the driver-specific data for this
//! display driver.
//! \param ulValue is the 24-bit RGB color. The least-significant byte is the
//! blue channel, the next byte is the green channel, and the third byte is the
//! red channel.
//!
//! This function translates a 24-bit RGB color into a value that can be
//! written into the display's frame buffer in order to reproduce that color,
//! or the closest possible approximation of that color.
//!
//! \return Returns the display-driver specific color.
//
//*****************************************************************************
static unsigned int
Kentec320x240x16_SSD2119ColorTranslate(void *pvDisplayData,
unsigned int ulValue)
{
//
// Translate from a 24-bit RGB color to a 5-6-5 RGB color.
//
return(DPYCOLORTRANSLATE(ulValue));
}
//*****************************************************************************
//
//! Flushes any cached drawing operations.
//!
//! \param pvDisplayData is a pointer to the driver-specific data for this
//! display driver.
//!
//! This functions flushes any cached drawing operations to the display. This
//! is useful when a local frame buffer is used for drawing operations, and the
//! flush would copy the local frame buffer to the display. For the SSD2119
//! driver, the flush is a no operation.
//!
//! \return None.
//
//*****************************************************************************
static void
Kentec320x240x16_SSD2119Flush(void *pvDisplayData)
{
//
// There is nothing to be done.
//
}
//*****************************************************************************
//
//! The display structure that describes the driver for the Kentec
//! K350QVG-V2-F TFT panel with an SSD2119 controller.
//
//*****************************************************************************
const tDisplay g_sKentec320x240x16_SSD2119 =
{
sizeof(tDisplay),
0,
#if defined(PORTRAIT) || defined(PORTRAIT_FLIP)
240,
320,
#else
320,
240,
#endif
Kentec320x240x16_SSD2119PixelDraw,
Kentec320x240x16_SSD2119PixelDrawMultiple,
Kentec320x240x16_SSD2119LineDrawH,
Kentec320x240x16_SSD2119LineDrawV,
Kentec320x240x16_SSD2119RectFill,
Kentec320x240x16_SSD2119ColorTranslate,
Kentec320x240x16_SSD2119Flush
};
//*****************************************************************************
//
// Close the Doxygen group.
//! @}
//
//*****************************************************************************