Other Parts Discussed in Thread: TMS570LS1114, HALCOGEN, TMS570LC4357
Hello,
I try to use the Flash EEPROM Emulation of the TMS570LS1114 device.
The HalCoGen (Version 04.03.00) generates the code for the access and the code of example_TI_Fee_Write_Read.c is copied into the ccs-project and the F021_API_CortexR4_BE_L2FMC_V3D16.lib is linked at the project settings.
The programm execution is stopped at the loop after the call of TI_Fee_Init(). The Status variable contains the value UNINIT.
I have searched for problems in the function TI_Fee_Init. At line 578 (ti_fee_ini.c) the function Fapi_initializeFlashBanks((uint32)TI_FEE_OPERATING_FREQUENCY)) returns the Fapi_StatusType Fapi_Error_OtpChecksumMismatch.
The HalCoGen Settings of the FEE are the default values.
Has anybody an idea to solve the problem?
sys_main.c
void main(void)
{
[...]
/* Initialize FEE. This will create Virtual sectors, initialize global variables etc.*/
TI_Fee_Init();
do
{
TI_Fee_MainFunction();
delay();
Status=TI_Fee_GetStatus(0 );
}
while(Status!= IDLE);
[...]
}