Other Parts Discussed in Thread: TMS570LS1114
Hello
The TMS570LS1114 datasheet states a maximum clock input frequency of 20 MHz. If I use a 20 MHz quarz oscillator with 100ppm tolerance over temperature is the device guaranteed to work?
Is there an absolute maximum input frequency you could state or at least a rough number where the limits are (i.e. 20.1 MHz / 20.5 MHz / 21.0 MHz)?
Best regards
Tobias