Other Parts Discussed in Thread: TM4C1294NCPDT
Hi all,
I thought I would just pop this question in here as I'm doing some tests myself. Has anybody noticed any difference when using the timer block to generate a PWM signal or when using the PWM block to generate a PWM signal on the TM4C1294NCPDT? I'm talking about mainly the resolution and accuracy of the signal.
I myself wouldn't think so because both of them use a 16bit timer, so using the same clock frequency there should be no difference, right?
Hopefully in this cary the theoretical case is closer to the practical case!