This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Filename and function name are not exact in trace with Trace Analyzer XDS560V2

Hello,
When I use the XDS560V2 Trace Analyzer the Filename column and Function name column are not always exact.
In the following trace the 2 last columns say what should be written in the two first columns.
What can be wrong in the use of XDS560V2 Trace Analyzer?
Thanks for your help
Jerome

Program Address:uinteger:hex                       Disassembly:string                                                                          Correct File         Correct Function
\HL_sys_startup.c                        _c_int00()        0x181DF0   CPSIE           f,                                                        \main_.asm        assmainTasks
\HL_sys_intvecs.asm                     adcInit()         0x1C           LDR             PC, 0xFFFFFE74                               Fetch FIQ vector     
\subroutines_interrupts.asm      saveAllReg()      0x60BC      STMFD           R13!, {R0, R1, R2, R3, R12, R14}   \HL_esm.c      esmHighInterrupt()
\subroutines_interrupts.asm      saveAllReg()      0x60C0      VMRS            R12, FPEXC                                     \HL_esm.c      esmHighInterrupt()
\subroutines_interrupts.asm      saveAllReg()      0x60C4      STMFD           R13!, {R12}                                      \HL_esm.c      esmHighInterrupt()
\subroutines_interrupts.asm      saveAllReg()      0x60C8      VMRS            R12, FPSCR                                     \HL_esm.c      esmHighInterrupt()
\subroutines_interrupts.asm      saveAllReg()      0x60CC      STMFD           R13!, {R12}                                      \HL_esm.c      esmHighInterrupt()
\subroutines_interrupts.asm      saveAllReg()      0x60D0      VSTMDB          R13!, {D0-D7}                                 \HL_esm.c      esmHighInterrupt()
\subroutines_interrupts.asm      saveAllReg()      0x60D4      SUB             R13, R13, #8                                       \HL_esm.c      esmHighInterrupt()
\subroutines_interrupts.asm      saveAllReg()      0x60D8      BL              0x5F14                                                  \HL_esm.c      esmHighInterrupt()
\subroutines_interrupts.asm      saveAllReg()      0x5F14      STMFD           R13!, {R4, R5, R6, R7, R8, R9, R10, R11}  \subroutines_interrupts.asm      saveAllReg()
\subroutines_interrupts.asm      saveAllReg()      0x5F18       BX              R14                                                      \subroutines_interrupts.asm      saveAllReg()
\subroutines_interrupts.asm      saveAllReg()      0x60DC      LDR             R8, 0x6230                                         \HL_esm.c      esmHighInterrupt()
\subroutines_interrupts.asm      saveAllReg()      0x60E0      LDR             R8, [R8]                                               \HL_esm.c      esmHighInterrupt()
\subroutines_interrupts.asm      saveAllReg()      0x60E4      SUB             R8, R8, #1                                           \HL_esm.c      esmHighInterrupt()
\subroutines_interrupts.asm      saveAllReg()      0x60E8      STR             R8, [R13]                                             \HL_esm.c      esmHighInterrupt()
\subroutines_interrupts.asm      saveAllReg()      0x60EC      LDR             R8, [R13]                                             \HL_esm.c      esmHighInterrupt()
\subroutines_interrupts.asm      saveAllReg()      0x60F0      CMP             R8, #32                                                \HL_esm.c      esmHighInterrupt()
\subroutines_interrupts.asm      saveAllReg()      0x60F4      BCS             0x611C                                                 \HL_esm.c      esmHighInterrupt()
\subroutines_interrupts.asm      saveAllReg()      0x611C      LDR             R8, [R13]                                              \HL_esm.c      esmHighInterrupt()
\subroutines_interrupts.asm      saveAllReg()      0x6120      CMP             R8, #64                                                \HL_esm.c      esmHighInterrupt()
\subroutines_interrupts.asm      saveAllReg()      0x6124      BCS             0x6154                                                 \HL_esm.c      esmHighInterrupt()
\subroutines_interrupts.asm      saveAllReg()      0x6128      LDR             R8, [R13]                                              \HL_esm.c      esmHighInterrupt()
\subroutines_interrupts.asm      saveAllReg()      0x612C      LDR             R10, 0x623C                                        \HL_esm.c      esmHighInterrupt()
\subroutines_interrupts.asm      saveAllReg()      0x6130      MOV             R9, #1                                                  \HL_esm.c      esmHighInterrupt()
\subroutines_interrupts.asm      saveAllReg()      0x6134      SUB             R8, R8, #32                                          \HL_esm.c      esmHighInterrupt()
\subroutines_interrupts.asm      saveAllReg()      0x6138      MOV             R8, R9, LSL R8                                   \HL_esm.c      esmHighInterrupt()
\subroutines_interrupts.asm      saveAllReg()      0x613C      STR             R8, [R10]                                             \HL_esm.c      esmHighInterrupt()
\subroutines_interrupts.asm      saveAllReg()      0x6140      LDR             R8, [R13]                                              \HL_esm.c      esmHighInterrupt()
\subroutines_interrupts.asm      saveAllReg()      0x6144      LDR             R0, 0x6238                                          \HL_esm.c      esmHighInterrupt()
\subroutines_interrupts.asm      saveAllReg()      0x6148      SUB             R1, R8, #32                                         \HL_esm.c      esmHighInterrupt()
\subroutines_interrupts.asm      saveAllReg()      0x614C      BL              0x55D0                                                 \HL_esm.c      esmHighInterrupt()
\HL_notification.c      esmGroup2Notification      0x55D0      SUB             R13, R13, #8                                       \HL_notification.c      esmGroup2Notification
\HL_notification.c      esmGroup2Notification      0x55D4      STR             R1, [R13, #4]                                       \HL_notification.c      esmGroup2Notification
\HL_notification.c      esmGroup2Notification      0x55D8      STR             R0, [R13]                                             \HL_notification.c      esmGroup2Notification
\HL_notification.c      esmGroup2Notification      0x55DC      ADD             R13, R13, #8                                      \HL_notification.c      esmGroup2Notification
\HL_notification.c      esmGroup2Notification      0x55E0      BX              R14                                                       \HL_notification.c      esmGroup2Notification
\subroutines_interrupts.asm      saveAllReg()      0x6150      B               0x620C                                                   \HL_esm.c      esmHighInterrupt()
\subroutines_interrupts.asm      saveAllReg()      0x620C      BL              0x5F1C                                                 \HL_esm.c      esmHighInterrupt()
\subroutines_interrupts.asm      saveAllReg()      0x5F1C      LDMFD           R13!, {R4, R5, R6, R7, R8, R9, R10, R11}  \subroutines_interrupts.asm      restrAllReg()
\subroutines_interrupts.asm      saveAllReg()      0x5F20      BX              R14                                                       \subroutines_interrupts.asm      restrAllReg()
\subroutines_interrupts.asm      saveAllReg()      0x6210      ADD             R13, R13, #8                                       \HL_esm.c      esmHighInterrupt()
\subroutines_interrupts.asm      saveAllReg()      0x6214      VMOV            R0, R13, D0                                      \HL_esm.c      esmHighInterrupt()
\subroutines_interrupts.asm      saveAllReg()      0x6218      LDMFD           R13!, {R12}                                      \HL_esm.c      esmHighInterrupt()
\subroutines_interrupts.asm      saveAllReg()      0x621C      VMSR            FPSCR, R12                                    \HL_esm.c      esmHighInterrupt()
\subroutines_interrupts.asm      saveAllReg()      0x6220      LDMFD           R13!, {R12}                                      \HL_esm.c      esmHighInterrupt()
\subroutines_interrupts.asm      saveAllReg()      0x6224      VMSR            FPEXC, R12                                     \HL_esm.c      esmHighInterrupt()
\subroutines_interrupts.asm      saveAllReg()      0x6228      LDMFD           R13!, {R0, R1, R2, R3, R12, R14}   \HL_esm.c      esmHighInterrupt()
\subroutines_interrupts.asm      saveAllReg()      0x622C      SUBS            PC, R14, #4                                      \HL_esm.c      esmHighInterrupt()
HL_sys_startup.c                   _c_int00()              0x181DF4  CPSIE          i,                                                         \main_.asm      assmainTasks