This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

HDK Connectivity Code on 3137 HDK - SD Card Code on SPI3 vs. SPI2?

Hello,

Took a look at the HDK Connectivity example for the 3137 HDK which is posted on that wiki.

From the schematic, the SD card is on SPI2 but in the example code that is on SPI3 - I guess this could be due to board change.

But, does that demo really do anything?  I tried adding a read_block command that returns an error.

Thanks in Advance,
johnw