Hi everyone, I´m using TMS570LS3137 microcontroller. It´s matricula printed over IC is listed below:
TMS570LS
3137CPGEQQ1
YFC-39AX5RW
G4
After turning on the PCB board, only the microcontroller begins to warm gradually.
A measurement of the impedance of the power supply node "3.3V", the value obtained corresponds to: 40 Ohms (doing the same measurement in a functional board, was obtained an impedance value of: 3.3 KOhms).
Similarly, the value of the impedance of the power node "1.2V", corresponds to 298 Ohms (doing the same measurement in a functional board, was obtained an impedance value of: 6.6KOhms).
Damaged PCB board counsumes 50mA more than a functional board.
We have not been able to identify exactly what might be the cause of the failure, since the values of the supply voltages of the microcontroller have the correct voltage. By now this failure is attributed to an internal short circuit into the microcontroller.
I have understood that this type of failure should be reported to the manufacturer to rule out any bug in this hardware version.
Please could you help me to identify a possible cause?
Who should I contact to follow up this failure?