Other Parts Discussed in Thread: HALCOGEN
Hello,
I am having the following error message from CCS when debug
CortexR5: GEL Output: Memory Map Setup for Flash @ Address 0x0CortexR5: GEL Output: Memory Map Setup for Flash @ Address 0x0 due to System Reset
CortexR5: Can't Run Target CPU: (Error -242 @ 0x0) A router subpath could not be accessed. The board configuration file is probably incorrect. (Emulation package 5.1.507.2)
Running CCS6.0.1, XDS100V2 14 pins from spectrum digital.
I found a discussion @ e2e.ti.com/.../395937
But I am not sure is the same questions is addressed/solved or not.
My JTAG connection
where PS5 = 3.42V.
Thanks