Other Parts Discussed in Thread: EK-TM4C1294XL, ISO1050
Hi everyone,
I have 8 motors to be controlled, all equipped with the integrated controller with the CANOpen protocol. There are two questions:
1. In principle, is it possible to control them by EK-TM4C1294XL + SimmaSoftware CANOpen library?
2. If yes than do I need any additional devices (like tranciever for example)? Are there any special booster packs with CAN connectivity function?
Thanks to all