Dear community,
I've got a problem with the GPIO port 5 and 6 (portbase C) on the TM4C123GH6PM.
Both ports are used to switch a MOSFET. Switching one MOSFET will affect a current flow through an insulation relay coil to close it.
By closing the first relay like that, there is sometimes no problem. When I try to swtich the second relay the scope shows, that the GPIO port goes up to 3,3V first.
The relay closes for a short period of 21ms. After this time the voltage sinks from 3,3V to ~1V at the GPIO port and holds this state. Sometimes the second gpio port also falls down to 1V and both relays open.
There is a pull-down resistor at every gpio output with a value of 33kOhm. Also there is a gate-source resistor with a value about 10kOhm.
Do you have any idea what is going on and how i can fix the issue?
Best regards,
Martin