This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Same outputs defined for several terminals for MMIO, intended?

I have a tms570lc4357hdk board from TI, 337ZWT Package.

In the IOMM table, some outputs are defined at several places, is this intended?

Example:

EXT_SEL[00] Is defined at W8 (address offset 170h) and at E16 (address offset 178h) 

Other examples are: N2HET2[20], MII_TX_CLK and a lot others.

This seems to many to be a mistake so it is intended?

Can you enable both at the same time?

Is the point just to provide another option if 2 outputs in the same terminal are wanted?