Other Parts Discussed in Thread: ENERGIA
Hello, I need to use a Nokia 5110 display with a TM4C123GXL TIVA for a project.
I found a ready with the implementation code. I copied the code snippets for just a single file, compiled and no error appears, but nothing is shown on the display screen. The pin-out as shown in this code, have re-checked everything. But my difficulty is to understand the code that actually appear the test text on the screen.
The code that I got to adapt this at this link (users.ece.utexas.edu/.../arm) -> Ctrl + F -> 5110
#include <stdint.h>
#include <stdbool.h>
#include "driverlib/sysctl.h"
//#include "inc/hw_memmap.h"
//#include "inc/hw_types.h"
//#include "inc/hw_gpio.h"
//#include "driverlib/gpio.h"
//#include "inc/tm4c123gh6pm.h"
//#include "driverlib/pin_map.h" //Mapping of peripherals to pins for all parts. "GPIOPinTypeUART"
//#include "driverlib/uart.h"
/* *************************** Pinagem | Pinou***************************
// Red SparkFun Nokia 5110 (LCD-10168)
-----------------------------------
Signal (Nokia 5110) LaunchPad pin
3.3V (VCC, pin 1) power
Ground (GND, pin 2) ground
SSI0Fss (SCE, pin 3) connected to PA3
Reset (RST, pin 4) connected to PA7
Data/Command (D/C, pin 5) connected to PA6
SSI0Tx (DN, pin 6) connected to PA5
SSI0Clk (SCLK, pin 7) connected to PA2
*/
/*
SYSDIV2 Divisor Clock (MHz)
0 1 reserved
1 2 reserved
2 3 reserved
3 4 reserved
4 5 80.000
5 6 66.667
6 7 reserved
7 8 50.000
8 9 44.444
9 10 40.000
10 11 36.364
11 12 33.333
12 13 30.769
13 14 28.571
14 15 26.667
15 16 25.000
16 17 23.529
17 18 22.222
18 19 21.053
19 20 20.000
20 21 19.048
21 22 18.182
22 23 17.391
23 24 16.667
24 25 16.000
25 26 15.385
26 27 14.815
27 28 14.286
28 29 13.793
29 30 13.333
30 31 12.903
31 32 12.500
32 33 12.121
33 34 11.765
34 35 11.429
35 36 11.111
36 37 10.811
37 38 10.526
38 39 10.256
39 40 10.000
40 41 9.756
41 42 9.524
42 43 9.302
43 44 9.091
44 45 8.889
45 46 8.696
46 47 8.511
47 48 8.333
48 49 8.163
49 50 8.000
50 51 7.843
51 52 7.692
52 53 7.547
53 54 7.407
54 55 7.273
55 56 7.143
56 57 7.018
57 58 6.897
58 59 6.780
59 60 6.667
60 61 6.557
61 62 6.452
62 63 6.349
63 64 6.250
64 65 6.154
65 66 6.061
66 67 5.970
67 68 5.882
68 69 5.797
69 70 5.714
70 71 5.634
71 72 5.556
72 73 5.479
73 74 5.405
74 75 5.333
75 76 5.263
76 77 5.195
77 78 5.128
78 79 5.063
79 80 5.000
80 81 4.938
81 82 4.878
82 83 4.819
83 84 4.762
84 85 4.706
85 86 4.651
86 87 4.598
87 88 4.545
88 89 4.494
89 90 4.444
90 91 4.396
91 92 4.348
92 93 4.301
93 94 4.255
94 95 4.211
95 96 4.167
96 97 4.124
97 98 4.082
98 99 4.040
99 100 4.000
100 101 3.960
101 102 3.922
102 103 3.883
103 104 3.846
104 105 3.810
105 106 3.774
106 107 3.738
107 108 3.704
108 109 3.670
109 110 3.636
110 111 3.604
111 112 3.571
112 113 3.540
113 114 3.509
114 115 3.478
115 116 3.448
116 117 3.419
117 118 3.390
118 119 3.361
119 120 3.333
120 121 3.306
121 122 3.279
122 123 3.252
123 124 3.226
124 125 3.200
125 126 3.175
126 127 3.150
127 128 3.125
*/
// *************************** Tamanho da tela | WINDOWS SIZE ***************************
#define SCREENW 84
#define SCREENH 48
// *************************** Definições | DEFINES ***************************
#define DC (*((volatile uint32_t *)0x40004100))
#define DC_COMMAND 0
#define DC_DATA 0x40
#define RESET (*((volatile uint32_t *)0x40004200))
#define RESET_LOW 0
#define RESET_HIGH 0x80
#define GPIO_PORTA_DIR_R (*((volatile uint32_t *)0x40004400))
#define GPIO_PORTA_AFSEL_R (*((volatile uint32_t *)0x40004420))
#define GPIO_PORTA_DEN_R (*((volatile uint32_t *)0x4000451C))
#define GPIO_PORTA_AMSEL_R (*((volatile uint32_t *)0x40004528))
#define GPIO_PORTA_PCTL_R (*((volatile uint32_t *)0x4000452C))
#define SSI0_CR0_R (*((volatile uint32_t *)0x40008000))
#define SSI0_CR1_R (*((volatile uint32_t *)0x40008004))
#define SSI0_DR_R (*((volatile uint32_t *)0x40008008))
#define SSI0_SR_R (*((volatile uint32_t *)0x4000800C))
#define SSI0_CPSR_R (*((volatile uint32_t *)0x40008010))
#define SSI0_CC_R (*((volatile uint32_t *)0x40008FC8))
#define SSI_CR0_SCR_M 0x0000FF00 // SSI Serial Clock Rate
#define SSI_CR0_SPH 0x00000080 // SSI Serial Clock Phase
#define SSI_CR0_SPO 0x00000040 // SSI Serial Clock Polarity
#define SSI_CR0_FRF_M 0x00000030 // SSI Frame Format Select
#define SSI_CR0_FRF_MOTO 0x00000000 // Freescale SPI Frame Format
#define SSI_CR0_DSS_M 0x0000000F // SSI Data Size Select
#define SSI_CR0_DSS_8 0x00000007 // 8-bit data
#define SSI_CR1_MS 0x00000004 // SSI Master/Slave Select
#define SSI_CR1_SSE 0x00000002 // SSI Synchronous Serial Port
// Enable
#define SSI_SR_BSY 0x00000010 // SSI Busy Bit
#define SSI_SR_TNF 0x00000002 // SSI Transmit FIFO Not Full
#define SSI_CPSR_CPSDVSR_M 0x000000FF // SSI Clock Prescale Divisor
#define SSI_CC_CS_M 0x0000000F // SSI Baud Clock Source
#define SSI_CC_CS_SYSPLL 0x00000000 // Either the system clock (if the
// PLL bypass is in effect) or the
// PLL output (default)
#define SYSCTL_RCGC1_R (*((volatile uint32_t *)0x400FE104))
#define SYSCTL_RCGC2_R (*((volatile uint32_t *)0x400FE108))
#define SYSCTL_RCGC1_SSI0 0x00000010 // SSI0 Clock Gating Control
#define SYSCTL_RCGC2_GPIOA 0x00000001 // port A Clock Gating Control
// *************************** Definições Nokia5110.h | MORE DEFINES ***************************
#define MAX_X 84
#define MAX_Y 48
#define CONTRAST 0xB1
// *************************** Definições PLL | DEFINES PLL ***************************
#define SYSCTL_RIS_R (*((volatile uint32_t *)0x400FE050))
#define SYSCTL_RIS_PLLLRIS 0x00000040 // PLL Lock Raw Interrupt Status
#define SYSCTL_RCC_R (*((volatile uint32_t *)0x400FE060))
#define SYSCTL_RCC_XTAL_M 0x000007C0 // Crystal Value
#define SYSCTL_RCC_XTAL_6MHZ 0x000002C0 // 6 MHz Crystal
#define SYSCTL_RCC_XTAL_8MHZ 0x00000380 // 8 MHz Crystal
#define SYSCTL_RCC_XTAL_16MHZ 0x00000540 // 16 MHz Crystal
#define SYSCTL_RCC2_R (*((volatile uint32_t *)0x400FE070))
#define SYSCTL_RCC2_USERCC2 0x80000000 // Use RCC2
#define SYSCTL_RCC2_DIV400 0x40000000 // Divide PLL as 400 MHz vs. 200
// MHz
#define SYSCTL_RCC2_SYSDIV2_M 0x1F800000 // System Clock Divisor 2
#define SYSCTL_RCC2_SYSDIV2LSB 0x00400000 // Additional LSB for SYSDIV2
#define SYSCTL_RCC2_PWRDN2 0x00002000 // Power-Down PLL 2
#define SYSCTL_RCC2_BYPASS2 0x00000800 // PLL Bypass 2
#define SYSCTL_RCC2_OSCSRC2_M 0x00000070 // Oscillator Source 2
#define SYSCTL_RCC2_OSCSRC2_MO 0x00000000 // MOSC
#define SYSDIV2 7
// *************************** Definições usadas no Exemplo ***************************
#define PIN_SCE 7 //Pin 3 on LCD
#define PIN_RESET 6 //Pin 4 on LCD
#define PIN_DC 5 //Pin 5 on LCD
#define PIN_SDIN 4 //Pin 6 on LCD
#define PIN_SCLK 3 //Pin 7 on LCD
//The DC pin tells the LCD if we are sending a command or data
#define LCD_COMMAND 0
#define LCD_DATA 1
//You may find a different size screen, but this one is 84 by 48 pixels
#define LCD_X 84
#define LCD_Y 48
// *************************** Enumerações, Constantes e Variáveis | ENUMS, CONSTANTS AND VARIABLES***************************
enum typeOfWrite{
COMMAND, // the transmission is an LCD command
DATA // the transmission is data
};
// This table contains the hex values that represent pixels
// for a font that is 5 pixels wide and 8 pixels high
static const uint8_t ASCII[][5] = {
{0x00, 0x00, 0x00, 0x00, 0x00} // 20
,{0x00, 0x00, 0x5f, 0x00, 0x00} // 21 !
,{0x00, 0x07, 0x00, 0x07, 0x00} // 22 "
,{0x14, 0x7f, 0x14, 0x7f, 0x14} // 23 #
,{0x24, 0x2a, 0x7f, 0x2a, 0x12} // 24 $
,{0x23, 0x13, 0x08, 0x64, 0x62} // 25 %
,{0x36, 0x49, 0x55, 0x22, 0x50} // 26 &
,{0x00, 0x05, 0x03, 0x00, 0x00} // 27 '
,{0x00, 0x1c, 0x22, 0x41, 0x00} // 28 (
,{0x00, 0x41, 0x22, 0x1c, 0x00} // 29 )
,{0x14, 0x08, 0x3e, 0x08, 0x14} // 2a *
,{0x08, 0x08, 0x3e, 0x08, 0x08} // 2b +
,{0x00, 0x50, 0x30, 0x00, 0x00} // 2c ,
,{0x08, 0x08, 0x08, 0x08, 0x08} // 2d -
,{0x00, 0x60, 0x60, 0x00, 0x00} // 2e .
,{0x20, 0x10, 0x08, 0x04, 0x02} // 2f /
,{0x3e, 0x51, 0x49, 0x45, 0x3e} // 30 0
,{0x00, 0x42, 0x7f, 0x40, 0x00} // 31 1
,{0x42, 0x61, 0x51, 0x49, 0x46} // 32 2
,{0x21, 0x41, 0x45, 0x4b, 0x31} // 33 3
,{0x18, 0x14, 0x12, 0x7f, 0x10} // 34 4
,{0x27, 0x45, 0x45, 0x45, 0x39} // 35 5
,{0x3c, 0x4a, 0x49, 0x49, 0x30} // 36 6
,{0x01, 0x71, 0x09, 0x05, 0x03} // 37 7
,{0x36, 0x49, 0x49, 0x49, 0x36} // 38 8
,{0x06, 0x49, 0x49, 0x29, 0x1e} // 39 9
,{0x00, 0x36, 0x36, 0x00, 0x00} // 3a :
,{0x00, 0x56, 0x36, 0x00, 0x00} // 3b ;
,{0x08, 0x14, 0x22, 0x41, 0x00} // 3c <
,{0x14, 0x14, 0x14, 0x14, 0x14} // 3d =
,{0x00, 0x41, 0x22, 0x14, 0x08} // 3e >
,{0x02, 0x01, 0x51, 0x09, 0x06} // 3f ?
,{0x32, 0x49, 0x79, 0x41, 0x3e} // 40 @
,{0x7e, 0x11, 0x11, 0x11, 0x7e} // 41 A
,{0x7f, 0x49, 0x49, 0x49, 0x36} // 42 B
,{0x3e, 0x41, 0x41, 0x41, 0x22} // 43 C
,{0x7f, 0x41, 0x41, 0x22, 0x1c} // 44 D
,{0x7f, 0x49, 0x49, 0x49, 0x41} // 45 E
,{0x7f, 0x09, 0x09, 0x09, 0x01} // 46 F
,{0x3e, 0x41, 0x49, 0x49, 0x7a} // 47 G
,{0x7f, 0x08, 0x08, 0x08, 0x7f} // 48 H
,{0x00, 0x41, 0x7f, 0x41, 0x00} // 49 I
,{0x20, 0x40, 0x41, 0x3f, 0x01} // 4a J
,{0x7f, 0x08, 0x14, 0x22, 0x41} // 4b K
,{0x7f, 0x40, 0x40, 0x40, 0x40} // 4c L
,{0x7f, 0x02, 0x0c, 0x02, 0x7f} // 4d M
,{0x7f, 0x04, 0x08, 0x10, 0x7f} // 4e N
,{0x3e, 0x41, 0x41, 0x41, 0x3e} // 4f O
,{0x7f, 0x09, 0x09, 0x09, 0x06} // 50 P
,{0x3e, 0x41, 0x51, 0x21, 0x5e} // 51 Q
,{0x7f, 0x09, 0x19, 0x29, 0x46} // 52 R
,{0x46, 0x49, 0x49, 0x49, 0x31} // 53 S
,{0x01, 0x01, 0x7f, 0x01, 0x01} // 54 T
,{0x3f, 0x40, 0x40, 0x40, 0x3f} // 55 U
,{0x1f, 0x20, 0x40, 0x20, 0x1f} // 56 V
,{0x3f, 0x40, 0x38, 0x40, 0x3f} // 57 W
,{0x63, 0x14, 0x08, 0x14, 0x63} // 58 X
,{0x07, 0x08, 0x70, 0x08, 0x07} // 59 Y
,{0x61, 0x51, 0x49, 0x45, 0x43} // 5a Z
,{0x00, 0x7f, 0x41, 0x41, 0x00} // 5b [
,{0x02, 0x04, 0x08, 0x10, 0x20} // 5c '\'
,{0x00, 0x41, 0x41, 0x7f, 0x00} // 5d ]
,{0x04, 0x02, 0x01, 0x02, 0x04} // 5e ^
,{0x40, 0x40, 0x40, 0x40, 0x40} // 5f _
,{0x00, 0x01, 0x02, 0x04, 0x00} // 60 `
,{0x20, 0x54, 0x54, 0x54, 0x78} // 61 a
,{0x7f, 0x48, 0x44, 0x44, 0x38} // 62 b
,{0x38, 0x44, 0x44, 0x44, 0x20} // 63 c
,{0x38, 0x44, 0x44, 0x48, 0x7f} // 64 d
,{0x38, 0x54, 0x54, 0x54, 0x18} // 65 e
,{0x08, 0x7e, 0x09, 0x01, 0x02} // 66 f
,{0x0c, 0x52, 0x52, 0x52, 0x3e} // 67 g
,{0x7f, 0x08, 0x04, 0x04, 0x78} // 68 h
,{0x00, 0x44, 0x7d, 0x40, 0x00} // 69 i
,{0x20, 0x40, 0x44, 0x3d, 0x00} // 6a j
,{0x7f, 0x10, 0x28, 0x44, 0x00} // 6b k
,{0x00, 0x41, 0x7f, 0x40, 0x00} // 6c l
,{0x7c, 0x04, 0x18, 0x04, 0x78} // 6d m
,{0x7c, 0x08, 0x04, 0x04, 0x78} // 6e n
,{0x38, 0x44, 0x44, 0x44, 0x38} // 6f o
,{0x7c, 0x14, 0x14, 0x14, 0x08} // 70 p
,{0x08, 0x14, 0x14, 0x18, 0x7c} // 71 q
,{0x7c, 0x08, 0x04, 0x04, 0x08} // 72 r
,{0x48, 0x54, 0x54, 0x54, 0x20} // 73 s
,{0x04, 0x3f, 0x44, 0x40, 0x20} // 74 t
,{0x3c, 0x40, 0x40, 0x20, 0x7c} // 75 u
,{0x1c, 0x20, 0x40, 0x20, 0x1c} // 76 v
,{0x3c, 0x40, 0x30, 0x40, 0x3c} // 77 w
,{0x44, 0x28, 0x10, 0x28, 0x44} // 78 x
,{0x0c, 0x50, 0x50, 0x50, 0x3c} // 79 y
,{0x44, 0x64, 0x54, 0x4c, 0x44} // 7a z
,{0x00, 0x08, 0x36, 0x41, 0x00} // 7b {
,{0x00, 0x00, 0x7f, 0x00, 0x00} // 7c |
,{0x00, 0x41, 0x36, 0x08, 0x00} // 7d }
,{0x10, 0x08, 0x08, 0x10, 0x08} // 7e ~
// ,{0x78, 0x46, 0x41, 0x46, 0x78} // 7f DEL
,{0x1f, 0x24, 0x7c, 0x24, 0x1f} // 7f UT sign
};
uint8_t Screen[SCREENW*SCREENH/8]; // buffer stores the next image to be printed on the screen
const unsigned char Masks[8]={0x01,0x02,0x04,0x08,0x10,0x20,0x40,0x80}; //usado na função Nokia5110_ClrPxl
// *************************** Protótipos Funções ***************************
void static lcdwrite(enum typeOfWrite type, uint8_t message);
void static lcddatawrite(uint8_t data);
void Nokia5110_Init(void);
void Nokia5110_OutChar(char data);
void Nokia5110_OutString(char *ptr);
void Nokia5110_OutUDec(uint16_t n);
void Nokia5110_SetCursor(uint8_t newX, uint8_t newY);
void Nokia5110_Clear(void);
void Nokia5110_DrawFullImage(const uint8_t *ptr);
void Nokia5110_PrintBMP(uint8_t xpos, uint8_t ypos, const uint8_t *ptr, uint8_t threshold);
void Nokia5110_ClearBuffer(void);
void Nokia5110_DisplayBuffer(void);
void Nokia5110_ClrPxl(uint32_t i, uint32_t j);
void Nokia5110_SetPxl(uint32_t i, uint32_t j);
void PLL_Init(void);
// *************************** exemplo main.c ***************************
int main(void){
uint32_t count = 0;
PLL_Init(); // set system clock to 50 MHz
Nokia5110_Init();
count = 0;
Nokia5110_Clear();
Nokia5110_OutString("************* LCD Test *************Letter: Num:------- ---- ");
Nokia5110_OutChar(127); // print UT sign
while(1){
Nokia5110_SetCursor(5, 5); // five leading spaces, bottom row
Nokia5110_OutChar((count%26)+'A');
Nokia5110_OutChar(' ');
Nokia5110_OutUDec(count);
SysCtlDelay(103333333); // delay ~0.5 sec at 50 MHz
count = count + 1;
}
}
/* *************************** main.c ***************************
*/
// *************************** Implementação Funções | Implementation of functions ***************************
// The Data/Command pin must be valid when the eighth bit is
// sent. The SSI module has hardware input and output FIFOs
// that are 8 locations deep. Based on the observation that
// the LCD interface tends to send a few commands and then a
// lot of data, the FIFOs are not used when writing
// commands, and they are used when writing data. This
// ensures that the Data/Command pin status matches the byte
// that is actually being transmitted.
// The write command operation waits until all data has been
// sent, configures the Data/Command pin for commands, sends
// the command, and then waits for the transmission to
// finish.
// The write data operation waits until there is room in the
// transmit FIFO, configures the Data/Command pin for data,
// and then adds the data to the transmit FIFO.
// This is a helper function that sends an 8-bit message to the LCD.
// inputs: type COMMAND or DATA
// message 8-bit code to transmit
// outputs: none
// assumes: SSI0 and port A have already been initialized and enabled
void static lcdwrite(enum typeOfWrite type, uint8_t message){
if(type == COMMAND){
// wait until SSI0 not busy/transmit FIFO empty
while((SSI0_SR_R&SSI_SR_BSY)==SSI_SR_BSY){};
DC = DC_COMMAND;
SSI0_DR_R = message; // command out
// wait until SSI0 not busy/transmit FIFO empty
while((SSI0_SR_R&SSI_SR_BSY)==SSI_SR_BSY){};
} else{
while((SSI0_SR_R&SSI_SR_TNF)==0){}; // wait until transmit FIFO not full
DC = DC_DATA;
SSI0_DR_R = message; // data out
}
}
void static lcddatawrite(uint8_t data){
while((SSI0_SR_R&0x00000002)==0){}; // wait until transmit FIFO not full
DC = DC_DATA;
SSI0_DR_R = data; // data out
}
//********Nokia5110_Init*****************
// Initialize Nokia 5110 48x84 LCD by sending the proper
// commands to the PCD8544 driver. One new feature of the
// LM4F120 is that its SSIs can get their baud clock from
// either the system clock or from the 16 MHz precision
// internal oscillator.
// inputs: none
// outputs: none
// assumes: system clock rate of 80 MHz
void Nokia5110_Init(void){
volatile uint32_t delay;
SYSCTL_RCGC1_R |= SYSCTL_RCGC1_SSI0; // activate SSI0
SYSCTL_RCGC2_R |= SYSCTL_RCGC2_GPIOA; // activate port A
delay = SYSCTL_RCGC2_R; // allow time to finish activating
GPIO_PORTA_DIR_R |= 0xC0; // make PA6,7 out
GPIO_PORTA_AFSEL_R |= 0x2C; // enable alt funct on PA2,3,5
GPIO_PORTA_AFSEL_R &= ~0xC0; // disable alt funct on PA6,7
GPIO_PORTA_DEN_R |= 0xEC; // enable digital I/O on PA2,3,5,6,7
// configure PA2,3,5 as SSI
GPIO_PORTA_PCTL_R = (GPIO_PORTA_PCTL_R&0xFF0F00FF)+0x00202200;
// configure PA6,7 as GPIO
GPIO_PORTA_PCTL_R = (GPIO_PORTA_PCTL_R&0x00FFFFFF)+0x00000000;
GPIO_PORTA_AMSEL_R &= ~0xEC; // disable analog functionality on PA2,3,5,6,7
SSI0_CR1_R &= ~SSI_CR1_SSE; // disable SSI
SSI0_CR1_R &= ~SSI_CR1_MS; // master mode
// configure for system clock/PLL baud clock source
SSI0_CC_R = (SSI0_CC_R&~SSI_CC_CS_M)+SSI_CC_CS_SYSPLL;
// clock divider for 3.33 MHz SSIClk (80 MHz PLL/24)
// SysClk/(CPSDVSR*(1+SCR))
// 80/(24*(1+0)) = 3.33 MHz (slower than 4 MHz)
SSI0_CPSR_R = (SSI0_CPSR_R&~SSI_CPSR_CPSDVSR_M)+24; // must be even number
SSI0_CR0_R &= ~(SSI_CR0_SCR_M | // SCR = 0 (3.33 Mbps data rate)
SSI_CR0_SPH | // SPH = 0
SSI_CR0_SPO); // SPO = 0
// FRF = Freescale format
SSI0_CR0_R = (SSI0_CR0_R&~SSI_CR0_FRF_M)+SSI_CR0_FRF_MOTO;
// DSS = 8-bit data
SSI0_CR0_R = (SSI0_CR0_R&~SSI_CR0_DSS_M)+SSI_CR0_DSS_8;
SSI0_CR1_R |= SSI_CR1_SSE; // enable SSI
RESET = RESET_LOW; // reset the LCD to a known state
for(delay=0; delay<10; delay=delay+1);// delay minimum 100 ns
RESET = RESET_HIGH; // negative logic
lcdwrite(COMMAND, 0x21); // chip active; horizontal addressing mode (V = 0); use extended instruction set (H = 1)
// set LCD Vop (contrast), which may require some tweaking:
lcdwrite(COMMAND, CONTRAST); // try 0xB1 (for 3.3V red SparkFun), 0xB8 (for 3.3V blue SparkFun), 0xBF if your display is too dark, or 0x80 to 0xFF if experimenting
lcdwrite(COMMAND, 0x04); // set temp coefficient
lcdwrite(COMMAND, 0x14); // LCD bias mode 1:48: try 0x13 or 0x14
lcdwrite(COMMAND, 0x20); // we must send 0x20 before modifying the display control mode
lcdwrite(COMMAND, 0x0C); // set display control to normal mode: 0x0D for inverse
}
//********Nokia5110_OutChar*****************
// Print a character to the Nokia 5110 48x84 LCD. The
// character will be printed at the current cursor position,
// the cursor will automatically be updated, and it will
// wrap to the next row or back to the top if necessary.
// One blank column of pixels will be printed on either side
// of the character for readability. Since characters are 8
// pixels tall and 5 pixels wide, 12 characters fit per row,
// and there are six rows.
// inputs: data character to print
// outputs: none
// assumes: LCD is in default horizontal addressing mode (V = 0)
void Nokia5110_OutChar(char data){int i;
lcddatawrite(0x00); // blank vertical line padding
for(i=0; i<5; i=i+1){
lcddatawrite(ASCII[data - 0x20][i]);
}
lcddatawrite(0x00); // blank vertical line padding
}
//********Nokia5110_OutString*****************
// Print a string of characters to the Nokia 5110 48x84 LCD.
// The string will automatically wrap, so padding spaces may
// be needed to make the output look optimal.
// inputs: ptr pointer to NULL-terminated ASCII string
// outputs: none
// assumes: LCD is in default horizontal addressing mode (V = 0)
void Nokia5110_OutString(char *ptr){
while(*ptr){
Nokia5110_OutChar((unsigned char)*ptr);
ptr = ptr + 1;
}
}
//********Nokia5110_OutUDec*****************
// Output a 16-bit number in unsigned decimal format with a
// fixed size of five right-justified digits of output.
// Inputs: n 16-bit unsigned number
// Outputs: none
// assumes: LCD is in default horizontal addressing mode (V = 0)
void Nokia5110_OutUDec(uint16_t n){
if(n < 10){
Nokia5110_OutString(" ");
Nokia5110_OutChar(n+'0'); /* n is between 0 and 9 */
} else if(n<100){
Nokia5110_OutString(" ");
Nokia5110_OutChar(n/10+'0'); /* tens digit */
Nokia5110_OutChar(n%10+'0'); /* ones digit */
} else if(n<1000){
Nokia5110_OutString(" ");
Nokia5110_OutChar(n/100+'0'); /* hundreds digit */
n = n%100;
Nokia5110_OutChar(n/10+'0'); /* tens digit */
Nokia5110_OutChar(n%10+'0'); /* ones digit */
}
else if(n<10000){
Nokia5110_OutChar(' ');
Nokia5110_OutChar(n/1000+'0'); /* thousands digit */
n = n%1000;
Nokia5110_OutChar(n/100+'0'); /* hundreds digit */
n = n%100;
Nokia5110_OutChar(n/10+'0'); /* tens digit */
Nokia5110_OutChar(n%10+'0'); /* ones digit */
}
else {
Nokia5110_OutChar(n/10000+'0'); /* ten-thousands digit */
n = n%10000;
Nokia5110_OutChar(n/1000+'0'); /* thousands digit */
n = n%1000;
Nokia5110_OutChar(n/100+'0'); /* hundreds digit */
n = n%100;
Nokia5110_OutChar(n/10+'0'); /* tens digit */
Nokia5110_OutChar(n%10+'0'); /* ones digit */
}
}
//********Nokia5110_SetCursor*****************
// Move the cursor to the desired X- and Y-position. The
// next character will be printed here. X=0 is the leftmost
// column. Y=0 is the top row.
// inputs: newX new X-position of the cursor (0<=newX<=11)
// newY new Y-position of the cursor (0<=newY<=5)
// outputs: none
void Nokia5110_SetCursor(uint8_t newX, uint8_t newY){
if((newX > 11) || (newY > 5)){ // bad input
return; // do nothing
}
// multiply newX by 7 because each character is 7 columns wide
lcdwrite(COMMAND, 0x80|(newX*7)); // setting bit 7 updates X-position
lcdwrite(COMMAND, 0x40|newY); // setting bit 6 updates Y-position
}
//********Nokia5110_Clear*****************
// Clear the LCD by writing zeros to the entire screen and
// reset the cursor to (0,0) (top left corner of screen).
// inputs: none
// outputs: none
void Nokia5110_Clear(void){
int i;
for(i=0; i<(MAX_X*MAX_Y/8); i=i+1){
lcddatawrite(0x00);
}
Nokia5110_SetCursor(0, 0);
}
//********Nokia5110_DrawFullImage*****************
// Fill the whole screen by drawing a 48x84 bitmap image.
// inputs: ptr pointer to 504 byte bitmap
// outputs: none
// assumes: LCD is in default horizontal addressing mode (V = 0)
void Nokia5110_DrawFullImage(const uint8_t *ptr){
int i;
Nokia5110_SetCursor(0, 0);
for(i=0; i<(MAX_X*MAX_Y/8); i=i+1){
lcddatawrite(ptr[i]);
}
}
uint8_t Screen[SCREENW*SCREENH/8]; // buffer stores the next image to be printed on the screen
//********Nokia5110_PrintBMP*****************
// Bitmaps defined above were created for the LM3S1968 or
// LM3S8962's 4-bit grayscale OLED display. They also
// still contain their header data and may contain padding
// to preserve 4-byte alignment. This function takes a
// bitmap in the previously described format and puts its
// image data in the proper location in the buffer so the
// image will appear on the screen after the next call to
// Nokia5110_DisplayBuffer();
// The interface and operation of this process is modeled
// after RIT128x96x4_BMP(x, y, image);
// inputs: xpos horizontal position of bottom left corner of image, columns from the left edge
// must be less than 84
// 0 is on the left; 82 is near the right
// ypos vertical position of bottom left corner of image, rows from the top edge
// must be less than 48
// 2 is near the top; 47 is at the bottom
// ptr pointer to a 16 color BMP image
// threshold grayscale colors above this number make corresponding pixel 'on'
// 0 to 14
// 0 is fine for ships, explosions, projectiles, and bunkers
// outputs: none
void Nokia5110_PrintBMP(uint8_t xpos, uint8_t ypos, const uint8_t *ptr, uint8_t threshold){
int32_t width = ptr[18], height = ptr[22], i, j;
uint16_t screenx, screeny;
uint8_t mask;
// check for clipping
if((height <= 0) || // bitmap is unexpectedly encoded in top-to-bottom pixel order
((width%2) != 0) || // must be even number of columns
((xpos + width) > SCREENW) || // right side cut off
(ypos < (height - 1)) || // top cut off
(ypos > SCREENH)) { // bottom cut off
return;
}
if(threshold > 14){
threshold = 14; // only full 'on' turns pixel on
}
// bitmaps are encoded backwards, so start at the bottom left corner of the image
screeny = ypos/8;
screenx = xpos + SCREENW*screeny;
mask = ypos%8; // row 0 to 7
mask = 0x01<<mask; // now stores a mask 0x01 to 0x80
j = ptr[10]; // byte 10 contains the offset where image data can be found
for(i=1; i<=(width*height/2); i=i+1){
// the left pixel is in the upper 4 bits
if(((ptr[j]>>4)&0xF) > threshold){
Screen[screenx] |= mask;
} else{
Screen[screenx] &= ~mask;
}
screenx = screenx + 1;
// the right pixel is in the lower 4 bits
if((ptr[j]&0xF) > threshold){
Screen[screenx] |= mask;
} else{
Screen[screenx] &= ~mask;
}
screenx = screenx + 1;
j = j + 1;
if((i%(width/2)) == 0){ // at the end of a row
if(mask > 0x01){
mask = mask>>1;
} else{
mask = 0x80;
screeny = screeny - 1;
}
screenx = xpos + SCREENW*screeny;
// bitmaps are 32-bit word aligned
switch((width/2)%4){ // skip any padding
case 0: j = j + 0; break;
case 1: j = j + 3; break;
case 2: j = j + 2; break;
case 3: j = j + 1; break;
}
}
}
}
// There is a buffer in RAM that holds one screen
// This routine clears this buffer
void Nokia5110_ClearBuffer(void){int i;
for(i=0; i<SCREENW*SCREENH/8; i=i+1){
Screen[i] = 0; // clear buffer
}
}
//********Nokia5110_DisplayBuffer*****************
// Fill the whole screen by drawing a 48x84 screen image.
// inputs: none
// outputs: none
// assumes: LCD is in default horizontal addressing mode (V = 0)
void Nokia5110_DisplayBuffer(void){
Nokia5110_DrawFullImage(Screen);
}
//------------Nokia5110_ClrPxl------------
// Clear the Image pixel at (i, j), turning it dark.
// Input: i the row index (0 to 47 in this case), y-coordinate
// j the column index (0 to 83 in this case), x-coordinate
// Output: none
void Nokia5110_ClrPxl(uint32_t i, uint32_t j){
Screen[84*(i>>3) + j] &= ~Masks[i&0x07];
}
//------------Nokia5110_SetPxl------------
// Set the Image pixel at (i, j), turning it on.
// Input: i the row index (0 to 47 in this case), y-coordinate
// j the column index (0 to 83 in this case), x-coordinate
// Output: none
void Nokia5110_SetPxl(uint32_t i, uint32_t j){
Screen[84*(i>>3) + j] |= Masks[i&0x07];
}
// configure the system to get its clock from the PLL
void PLL_Init(void){
// 0) configure the system to use RCC2 for advanced features
// such as 400 MHz PLL and non-integer System Clock Divisor
SYSCTL_RCC2_R |= SYSCTL_RCC2_USERCC2;
// 1) bypass PLL while initializing
SYSCTL_RCC2_R |= SYSCTL_RCC2_BYPASS2;
// 2) select the crystal value and oscillator source
SYSCTL_RCC_R &= ~SYSCTL_RCC_XTAL_M; // clear XTAL field
SYSCTL_RCC_R += SYSCTL_RCC_XTAL_16MHZ;// configure for 16 MHz crystal
SYSCTL_RCC2_R &= ~SYSCTL_RCC2_OSCSRC2_M;// clear oscillator source field
SYSCTL_RCC2_R += SYSCTL_RCC2_OSCSRC2_MO;// configure for main oscillator source
// 3) activate PLL by clearing PWRDN
SYSCTL_RCC2_R &= ~SYSCTL_RCC2_PWRDN2;
// 4) set the desired system divider and the system divider least significant bit
SYSCTL_RCC2_R |= SYSCTL_RCC2_DIV400; // use 400 MHz PLL
SYSCTL_RCC2_R = (SYSCTL_RCC2_R&~0x1FC00000) // clear system clock divider field
+ (SYSDIV2<<22); // configure for 80 MHz clock
// 5) wait for the PLL to lock by polling PLLLRIS
while((SYSCTL_RIS_R&SYSCTL_RIS_PLLLRIS)==0){};
// 6) enable use of PLL by clearing BYPASS
SYSCTL_RCC2_R &= ~SYSCTL_RCC2_BYPASS2;
}