This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

using IAR I-jet with DK-TM4C129X dev kit

I have been running my TI dev kit via the ICDI USB port until now, but just got an I-jet debugger from IAR and am trying to configure things to work with it. I changed the Project Options/Debugger settings to use "I-jet/JTAGjet" instead of "TI Stellaris". But when I try to download my code I get an error saying "Fatal error: Couldn't power up the target board - probably a shorted circuit."

I have tried all combinations of jumpers on J11 (none, 1-to-2 and 2-3) and get the same error regardless. Any idea what I need to do to get the I-jet working?

Thanks,

Dave