Other Parts Discussed in Thread: TM4C123GH6PM, TM4C1294NCPDT
I have written the program given below which is working perfectly with TM4C123gh6pm but the program get stuck in "while(I2CMasterBusy(I2C0_BASE))" when running in TM4C1294NCPDT.
Can anyone help???
void RTC_WRITE()
{
while(run_once)
{
I2CMasterSlaveAddrSet(I2C0_BASE, 0x68, false); // The address of the Slave is 0x68
I2CMasterDataPut(I2C0_BASE, RTCRegister); // Addr 0x00
I2CMasterControl(I2C0_BASE, I2C_MASTER_CMD_BURST_SEND_START);
while(!(I2CMasterBusy(I2C0_BASE)));
while(I2CMasterBusy(I2C0_BASE));
// SysCtlDelay(3000);
for (i=0;i<7;i++)
{
I2CMasterDataPut(I2C0_BASE, RTCSetup[i]);
I2CMasterControl(I2C0_BASE, I2C_MASTER_CMD_BURST_SEND_CONT);
while(!(I2CMasterBusy(I2C0_BASE)));
while(I2CMasterBusy(I2C0_BASE));
}
I2CMasterControl(I2C0_BASE, I2C_MASTER_CMD_BURST_SEND_FINISH );
while(!(I2CMasterBusy(I2C0_BASE)));
while(I2CMasterBusy(I2C0_BASE));
run_once = false;
}
SysCtlDelay(550000); // writing time
}
int main(void)
{
uint32_t FREQ=0;
FREQ=SysCtlClockFreqSet((SYSCTL_XTAL_25MHZ | SYSCTL_OSC_MAIN | SYSCTL_USE_PLL |SYSCTL_CFG_VCO_480), 120000000);
SysCtlPeripheralEnable(SYSCTL_PERIPH_I2C0);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOB);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOD);//LCD
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOQ);//LCD
GPIOPinTypeI2CSCL(GPIO_PORTB_BASE, GPIO_PIN_2); // I2CSCL
GPIOPinTypeI2C(GPIO_PORTB_BASE, GPIO_PIN_3);
GPIOPinConfigure(GPIO_PB2_I2C0SCL);
GPIOPinConfigure(GPIO_PB3_I2C0SDA);
I2CMasterInitExpClk(I2C0_BASE, FREQ, false);
GPIOPinTypeGPIOOutput(GPIO_PORTD_BASE, GPIO_PIN_0|GPIO_PIN_1|GPIO_PIN_2|GPIO_PIN_3|GPIO_PIN_4|GPIO_PIN_5|GPIO_PIN_6|GPIO_PIN_7);
GPIOPinTypeGPIOOutput(GPIO_PORTQ_BASE, GPIO_PIN_0|GPIO_PIN_1);
SysCtlDelay(2000000);
LCD_INT();
RTC_WRITE();
while(1)
{
RTC_READ();
}
}