Other Parts Discussed in Thread: TM4C123GH6PM
I recently had a circuit board made with a TM4C123GH6PM on it. When I apply power, the current on the power supply approaches 1 Amp. The TM4C123GH6PM is powered off a 3.3V linear regulator. I am trying to apply 5V to the input of the regulator, but as soon as it gets close to about 2.5V, the current shoots up and the TM4C123GH6PM gets hot.
My plan was to power it up, then connect a JTAG and program it. I've removed mostly everything else from the board that might cause problems.
What am I doing wrong? Should the /RESET or other pins be held at a certain state while the chip is blank?