Other Parts Discussed in Thread: TM4C129XNCZAD, MAX232
Hi All:
I've written some programs using UART, I2C, ADC, etc features for both of the Tiva Launch Pad boards with no issues.
Due to some appealing features, I decided to take a look at the Easy MX Pro v7 board from MikroElectronika using the TM4C129XNCZAD chip.
I am using Code Composer 6.1, TI-RTOS with UART drivers with the Easy MX Pro hardware.
I can Load and Debug my program from the board; but, I can not get the UARTs to do anything. I've tried all 8 sets of UART PINS. Nothing.
I followed all of the recommendation on the Wiki. The UART example is 'dated'.
I believe the Tiva Launchpads use a 25Mhz Oscillator along with the Mikro board.
Does anyone have any experience with this board? Did you get these working together? Is this a lost cause?
Thanks
Rick