Other Parts Discussed in Thread: RM46L852
Hi,
According to the SPNS185C manual :
B2 pin can be used for : MIBSPI3NCS[2] / I2C_SDA / N2HET1[27] / nTZ2
C3 pin can be used for : MIBSPI3NCS[3] / I2C_SCL / N2HET1[29] / nTZ1
But pin A9 is also used for N2HET1[27] (and this is the unique function on this pin)
and pin A3 is also used for N2HET1[29] (and this is the unique function on this pin)
So there is something I don't understand: how is it possible to use the B2 pin as N2HET1[27] as this function is allocated to the A9 pin?
Same question for C3 and A3 pins.
Thanks for help.
Bruno