Other Parts Discussed in Thread: RM48L952, RM44L520
Hello,
I am migrating code from RM48L952 to Rm44l520.
Hardware: I have completed the function inspection under RM48L952. Then I change the MCU from RM48L952 to RM44L520. (Main OSC still is 20MHz). JTAG interface have passed the test by the button "test connection' in CCS6.1.
Tools: CCS6.1, HalCoGen04.04, XDS100V2.
Code: The code was generated by HalCoGen04.04 with a rm44l520pge setup, and it passed the "build all'
Problem: When I download the code to the rm44l520, I got a error information showed below.
Is there someone knows what the error information for?
Thanks,
Dison