This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EPI Clock Absent on TM4C129XL

Hi,

I am adding a synchronous FIFO to the EPI, and require the EPI clock on EPIOS31. The clock is referenced in the timing diagrams, but is mysteriously absent from the aforementioned pin. Is there a special initialization required to enable it? I note that there is a library parameter to invert it (EPI_HB8_CLOCK_INVERT). I am using the ROM_EPIConfigHB8Set configuration as follows:

ROM_EPIConfigHB8Set(EPI0_BASE, EPI_HB8_MODE_ADMUX | EPI_HB8_WRWAIT_0
| EPI_HB8_CSCFG_ALE | EPI_HB8_ALE_LOW | EPI_HB8_CLOCK_INVERT
| EPI_HB8_RDWAIT_0 | EPI_HB8_CSCFG_CS, 0);

I would appreciate any assistance.

Thanks,

Joe

  • Hello Joe,

    Have you configured the GPIO corresponding to EPI Pin 31 for EPI function using GPIOPinConfigure and GPIOPinTypeEPI API calls?

    Also can you share the full EPI Configuration?

    Regards
    Amit
  • Joseph Curasi said:
    ...clock is referenced in the timing diagrams, but is mysteriously absent ...from the pin 

    Surely Amit's post "nails" this - yet we must note that vital "set-up/config code" - key in resolution - also is, "mysteriously absent!"

  • Hello cb1,

    Yes indeed. The full configuration is required as well.

    Regards
    Amit
  • Hi Amit,

    Yes, I omitted the EPICLK configuration statements. Here is the complete setup:

    // Enable the EPI peripheral
    ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_EPI0);

    //---------------------------------------------------------------
    // GPIO PORTS USED FOR EPI
    //---------------------------------------------------------------

    ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);
    ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOB);
    ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOC);
    ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOG);
    ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOK);
    ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOL);
    ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOM);
    ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOP);
    ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOQ);



    // Address Data Bus (AD7:AD0)
    ROM_GPIOPinConfigure(GPIO_PK0_EPI0S0); // AD0
    GPIOPinTypeEPI(GPIO_PORTK_BASE, GPIO_PIN_0);

    ROM_GPIOPinConfigure(GPIO_PK1_EPI0S1);
    GPIOPinTypeEPI(GPIO_PORTK_BASE, GPIO_PIN_1);

    ROM_GPIOPinConfigure(GPIO_PK2_EPI0S2);
    GPIOPinTypeEPI(GPIO_PORTK_BASE, GPIO_PIN_2);

    ROM_GPIOPinConfigure(GPIO_PK3_EPI0S3);
    GPIOPinTypeEPI(GPIO_PORTK_BASE, GPIO_PIN_3);

    ROM_GPIOPinConfigure(GPIO_PC7_EPI0S4);
    GPIOPinTypeEPI(GPIO_PORTC_BASE, GPIO_PIN_7);

    ROM_GPIOPinConfigure(GPIO_PC6_EPI0S5);
    GPIOPinTypeEPI(GPIO_PORTC_BASE, GPIO_PIN_6);

    ROM_GPIOPinConfigure(GPIO_PC5_EPI0S6);
    GPIOPinTypeEPI(GPIO_PORTC_BASE, GPIO_PIN_5);

    ROM_GPIOPinConfigure(GPIO_PC4_EPI0S7); // AD7
    GPIOPinTypeEPI(GPIO_PORTC_BASE, GPIO_PIN_4);

    // Control Signals
    ROM_GPIOPinConfigure(GPIO_PP3_EPI0S30); // nALE
    GPIOPinTypeEPI(GPIO_PORTP_BASE, GPIO_PIN_3);

    ROM_GPIOPinConfigure(GPIO_PP2_EPI0S29); // nWR
    GPIOPinTypeEPI(GPIO_PORTP_BASE, GPIO_PIN_2);

    ROM_GPIOPinConfigure(GPIO_PB3_EPI0S28); // nOE
    GPIOPinTypeEPI(GPIO_PORTB_BASE, GPIO_PIN_3);

    ROM_GPIOPinConfigure(GPIO_PK5_EPI0S31); // EPICLK
    GPIOPinTypeEPI(GPIO_PORTK_BASE, GPIO_PIN_5);


    // Address Bus (A20:A8)
    ROM_GPIOPinConfigure(GPIO_PA6_EPI0S8); // A8
    GPIOPinTypeEPI(GPIO_PORTA_BASE, GPIO_PIN_6);

    ROM_GPIOPinConfigure(GPIO_PA7_EPI0S9);
    GPIOPinTypeEPI(GPIO_PORTA_BASE, GPIO_PIN_7);

    ROM_GPIOPinConfigure(GPIO_PG1_EPI0S10);
    GPIOPinTypeEPI(GPIO_PORTG_BASE, GPIO_PIN_1);

    ROM_GPIOPinConfigure(GPIO_PG0_EPI0S11);
    GPIOPinTypeEPI(GPIO_PORTG_BASE, GPIO_PIN_0);

    ROM_GPIOPinConfigure(GPIO_PM3_EPI0S12);
    GPIOPinTypeEPI(GPIO_PORTM_BASE, GPIO_PIN_3);

    ROM_GPIOPinConfigure(GPIO_PM2_EPI0S13);
    GPIOPinTypeEPI(GPIO_PORTM_BASE, GPIO_PIN_2);

    ROM_GPIOPinConfigure(GPIO_PM1_EPI0S14);
    GPIOPinTypeEPI(GPIO_PORTM_BASE, GPIO_PIN_1);

    ROM_GPIOPinConfigure(GPIO_PM0_EPI0S15);
    GPIOPinTypeEPI(GPIO_PORTM_BASE, GPIO_PIN_0);

    ROM_GPIOPinConfigure(GPIO_PL0_EPI0S16);
    GPIOPinTypeEPI(GPIO_PORTL_BASE, GPIO_PIN_0);

    ROM_GPIOPinConfigure(GPIO_PL1_EPI0S17);
    GPIOPinTypeEPI(GPIO_PORTL_BASE, GPIO_PIN_1);

    ROM_GPIOPinConfigure(GPIO_PL2_EPI0S18);
    GPIOPinTypeEPI(GPIO_PORTL_BASE, GPIO_PIN_2);

    ROM_GPIOPinConfigure(GPIO_PL3_EPI0S19);
    GPIOPinTypeEPI(GPIO_PORTL_BASE, GPIO_PIN_3);

    ROM_GPIOPinConfigure(GPIO_PQ0_EPI0S20);
    GPIOPinTypeEPI(GPIO_PORTQ_BASE, GPIO_PIN_0); // A20





    //---------------------------------------------------------------
    // EPI Setup
    //---------------------------------------------------------------

    // Set the EPI divider.
    ROM_EPIDividerSet(EPI0_BASE, 1); // Set to 1 (Do not set to 0)

    // Select EPI Host Bus 8-bit mode.
    ROM_EPIModeSet(EPI0_BASE, EPI_MODE_HB8);

    // Configure SRAM mode
    // EPIConfigHB8Set - all data transfers use bits[7:0]
    ROM_EPIConfigHB8Set(EPI0_BASE, EPI_HB8_MODE_ADMUX | EPI_HB8_WRWAIT_0
    | EPI_HB8_CSCFG_ALE | EPI_HB8_ALE_LOW
    | EPI_HB8_RDWAIT_0 | EPI_HB8_CSCFG_CS, 0);


    // Set the address map. Base 0x6000 0000, Using 1MB out of 16MB addr space
    // Addr 0x6000 0000 - 1 Mbyte SRAM
    // Addr 0x6010 0000 - 32Kx9 FIFO
    ROM_EPIAddressMapSet(EPI0_BASE, EPI_ADDR_RAM_SIZE_16MB | EPI_ADDR_RAM_BASE_6);

    Thank you for your extremely quick response,

    Joe

  • Hello Joe,

    So now is it working? I tried the same on my setup and PK5 toggles as a clock

    Regards
    Amit
  • Hi Amit,

    My ALE demux (~ '373) in my CPLD is not working properly. I noted that I set both EPI_HB8_CSCFG_ALE and EPI_HB8_CSCFG_CS for pin EPIS030. I fixed it as shown below, however I still receive a recurring pattern of bit errors. Is the entire EPI configuration OK now? I use A20 for the chip select, so it is always low when addressing the SRAM.

    // Configure SRAM mode
    // EPIConfigHB8Set - all data transfers use bits[7:0]
    // ROM_EPIConfigHB8Set(EPI0_BASE, EPI_HB8_MODE_ADMUX | EPI_HB8_WRWAIT_0
    // | EPI_HB8_CSCFG_ALE | EPI_HB8_ALE_LOW
    // | EPI_HB8_RDWAIT_0 | EPI_HB8_CSCFG_CS, 0);

    ROM_EPIConfigHB8Set(EPI0_BASE, EPI_HB8_MODE_ADMUX | EPI_HB8_WRWAIT_0
    | EPI_HB8_CSCFG_ALE | EPI_HB8_ALE_LOW
    | EPI_HB8_RDWAIT_0, 0); // 7-8-15

    Thanks,

    Joe

  • Hello Joe

    Why are you using A20 for Chip Select when that is a separate signal in the ADMUX mode?

    Regards
    Amit
  • Hi Amit,

    The SRAM utilizes addresses A19:A0 (1 Mbyte), so A20 is the next available address. When A20 is low it selects my SRAM; when high it selects my FIFO. It seems like a simple addressing scheme - that's why I chose it. Is there any disadvantages when using this with the TM4C129? (The ALE signal uses my CS on EPISO30).

    Thanks,

    Joe

  • Hello Joe,

    Can you please share the schematics. It would be easier for me to correlate the code operation. Note that since this ADMUX the Address will not last for the entire cycle so the A20 may be lost after address phase.

    Regards
    Amit
  • Hi Amit,

    I modified the circuit so that CS0 is wired to the SRAM, and CS1 to the FIFO. I am operating in the EPI_HB8_CSCFG_ALE_DUAL_CS mode. (I no longer use A20 as part of my chip select logic). After configuring the EPI pins for this mode, I do not receive a chip select on the SRAM. Here is the full EPI setup once again:

    // Enable the EPI peripheral
    ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_EPI0);

    //---------------------------------------------------------------
    // GPIO PORTS USED FOR EPI
    //---------------------------------------------------------------

    ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);
    ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOB);
    ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOC);
    ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOG);
    ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOK);
    ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOL);
    ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOM);
    ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOP);
    ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOQ);



    // Address Data Bus (AD7:AD0)
    ROM_GPIOPinConfigure(GPIO_PK0_EPI0S0); // AD0
    GPIOPinTypeEPI(GPIO_PORTK_BASE, GPIO_PIN_0);

    ROM_GPIOPinConfigure(GPIO_PK1_EPI0S1);
    GPIOPinTypeEPI(GPIO_PORTK_BASE, GPIO_PIN_1);

    ROM_GPIOPinConfigure(GPIO_PK2_EPI0S2);
    GPIOPinTypeEPI(GPIO_PORTK_BASE, GPIO_PIN_2);

    ROM_GPIOPinConfigure(GPIO_PK3_EPI0S3);
    GPIOPinTypeEPI(GPIO_PORTK_BASE, GPIO_PIN_3);

    ROM_GPIOPinConfigure(GPIO_PC7_EPI0S4);
    GPIOPinTypeEPI(GPIO_PORTC_BASE, GPIO_PIN_7);

    ROM_GPIOPinConfigure(GPIO_PC6_EPI0S5);
    GPIOPinTypeEPI(GPIO_PORTC_BASE, GPIO_PIN_6);

    ROM_GPIOPinConfigure(GPIO_PC5_EPI0S6);
    GPIOPinTypeEPI(GPIO_PORTC_BASE, GPIO_PIN_5);

    ROM_GPIOPinConfigure(GPIO_PC4_EPI0S7); // AD7
    GPIOPinTypeEPI(GPIO_PORTC_BASE, GPIO_PIN_4);

    // Control Signals
    ROM_GPIOPinConfigure(GPIO_PP3_EPI0S30); // nALE
    GPIOPinTypeEPI(GPIO_PORTP_BASE, GPIO_PIN_3);

    ROM_GPIOPinConfigure(GPIO_PP2_EPI0S29); // nWR
    GPIOPinTypeEPI(GPIO_PORTP_BASE, GPIO_PIN_2);

    ROM_GPIOPinConfigure(GPIO_PB3_EPI0S28); // nOE
    GPIOPinTypeEPI(GPIO_PORTB_BASE, GPIO_PIN_3);

    ROM_GPIOPinConfigure(GPIO_PK5_EPI0S31); // EPICLK
    GPIOPinTypeEPI(GPIO_PORTK_BASE, GPIO_PIN_5);

    // S26 CS1 [PL4]
    ROM_GPIOPinConfigure(GPIO_PL4_EPI0S26);
    GPIOPinTypeEPI(GPIO_PORTL_BASE, GPIO_PIN_4);


    // S27 CS0 [PB2]
    ROM_GPIOPinConfigure(GPIO_PB2_EPI0S27);
    GPIOPinTypeEPI(GPIO_PORTB_BASE, GPIO_PIN_2);


    // Address Bus (A20:A8)
    ROM_GPIOPinConfigure(GPIO_PA6_EPI0S8); // A8
    GPIOPinTypeEPI(GPIO_PORTA_BASE, GPIO_PIN_6);

    ROM_GPIOPinConfigure(GPIO_PA7_EPI0S9);
    GPIOPinTypeEPI(GPIO_PORTA_BASE, GPIO_PIN_7);

    ROM_GPIOPinConfigure(GPIO_PG1_EPI0S10);
    GPIOPinTypeEPI(GPIO_PORTG_BASE, GPIO_PIN_1);

    ROM_GPIOPinConfigure(GPIO_PG0_EPI0S11);
    GPIOPinTypeEPI(GPIO_PORTG_BASE, GPIO_PIN_0);

    ROM_GPIOPinConfigure(GPIO_PM3_EPI0S12);
    GPIOPinTypeEPI(GPIO_PORTM_BASE, GPIO_PIN_3);

    ROM_GPIOPinConfigure(GPIO_PM2_EPI0S13);
    GPIOPinTypeEPI(GPIO_PORTM_BASE, GPIO_PIN_2);

    ROM_GPIOPinConfigure(GPIO_PM1_EPI0S14);
    GPIOPinTypeEPI(GPIO_PORTM_BASE, GPIO_PIN_1);

    ROM_GPIOPinConfigure(GPIO_PM0_EPI0S15);
    GPIOPinTypeEPI(GPIO_PORTM_BASE, GPIO_PIN_0);

    ROM_GPIOPinConfigure(GPIO_PL0_EPI0S16);
    GPIOPinTypeEPI(GPIO_PORTL_BASE, GPIO_PIN_0);

    ROM_GPIOPinConfigure(GPIO_PL1_EPI0S17);
    GPIOPinTypeEPI(GPIO_PORTL_BASE, GPIO_PIN_1);

    ROM_GPIOPinConfigure(GPIO_PL2_EPI0S18);
    GPIOPinTypeEPI(GPIO_PORTL_BASE, GPIO_PIN_2);

    ROM_GPIOPinConfigure(GPIO_PL3_EPI0S19);
    GPIOPinTypeEPI(GPIO_PORTL_BASE, GPIO_PIN_3);

    ROM_GPIOPinConfigure(GPIO_PQ0_EPI0S20);
    GPIOPinTypeEPI(GPIO_PORTQ_BASE, GPIO_PIN_0); // A20





    //---------------------------------------------------------------
    // EPI Setup
    //---------------------------------------------------------------

    // Set the EPI divider.
    ROM_EPIDividerSet(EPI0_BASE, 1); // Set to 1 (Do not set to 0)

    // Select EPI Host Bus 8-bit mode.
    ROM_EPIModeSet(EPI0_BASE, EPI_MODE_HB8);

    // Configure SRAM mode
    // EPIConfigHB8Set - all data transfers use bits[7:0]
    ROM_EPIConfigHB8Set(EPI0_BASE, EPI_HB8_MODE_ADMUX | EPI_HB8_WRWAIT_0
    | EPI_HB8_CSCFG_ALE_DUAL_CS | EPI_HB8_ALE_LOW // 7-13
    | EPI_HB8_RDWAIT_0, 0); // 7-10-15 note - "2" wait states on both read and write

    // Set the address map. Base 0x6000 0000, Using 1MB out of 16MB addr space
    // Addr 0x6000 0000 - 1 Mbyte SRAM (cs0)
    // Addr 0x6 - 32Kx9 FIFO (cs1)


    ROM_EPIAddressMapSet(EPI0_BASE, EPI_ADDR_RAM_SIZE_16MB | EPI_ADDR_RAM_BASE_6);

    1) Why don't I have a CS0 chip select?

    2) What would be the base address for the FIFO chip select?

    (I refereed to the TM4C129x ROM User's Guide.)

    Thanks,

    Joe

     

  • Hello Joe,

    I think this thread will explain the issue.

    e2e.ti.com/.../431469

    Can you enable the Peripheral region Address map by writing 0x99 to EPIADDRMAP and then accessing the address space of 0xA000.0000

    Alternatively route the nCS1 to RAM Chip Select on the CPLD and vice versa for nCS0.

    Regards
    Amit
  • Hi Amit,

    After swapping the addresses as you suggested, the SRAM  (unfortunately) behaves identical as when I used ADDR20 to select between the SRAM and the FIFO. The timing on the EPI bus does not appear as I expect. When I write 0x55 to all 1M locations I receive back a count - apparently the address feeding back into the data field. It would appear as if I have a configuration parameter incorrect.

    Thanks,

    Joe

  • Hello Joe,

    I think we need to probe the signals going to the SRAM to see what is happening.

    Regards
    Amit
  • Hi Amit,

    The wrong SRAM was received and installed on the board. Rather than a   IS61WV10248BLL-10TLI   it was a IS62WV10248DBLL-55TLI. The distributor mixed both parts in the same package that we received.

    Thanks for your help, and sorry about the false alarm.

    Joe

  • Hello Joe,

    If it helps, I also made a similar mistake when instead of ordering the DBLL package I ordered the DALL package.

    Regards
    Amit
  • Feel not bad guys - this reporter (and smarter cohorts) have "bin boxes" filled w/Not quite "Good for Gov't Work" devices - ("off" by single char in most cases & discovered "too late" to return/exchange!) Hate when that happens - Devil delights in such detail...