Other Parts Discussed in Thread: RM44L520, RM48L952
Hi there,
I testing every pins status of RM44L520 MCU of my PCB, because I can not download code to MCU, although it have passed the test connection inspection for JTAG.
The all of OSC, PRO-RESET, REST, every power supply pins and ground pins are correct, expect N-error pin which is low. I think the low N-error is the reason that download code failure.
My questions is
q1: What can make the n-error come on. The MCU still is empty, so there is not any wrong from code and setup. And the pins of MCU have been test one by one, there is any pin short or open. Power supply are all correct which are 3v29 and 1v18.
q2:Whether the MCU can be concluded that was damaged.
q3: Is there any way to test the MCU is good or not?
Thanks,
Dison