Other Parts Discussed in Thread: TMS570LC4357
The TMS570LC4357 contains multiple switches that can be used to calibrate the A/D offset. Should the ADREFLO be used or the mid-point value compared to ADREFHI/2? My first thought was to use the ADREFLO as the offset calibration, then use the mid-point calibration to develop a gain correction constant. The constant would be multiplied with the conversion results from the analog inputs to adjust for gain errors. However the use of ADREFLO is only useful if the offset is guaranteed to be one direction.
What is the preferred method which results in the least error?
Thanks,
Tom