Other Parts Discussed in Thread: EK-TM4C123GXL, TM4C123GH6PM
Dear Sir/Madam,
Following is the Console messages while builiding Lab2 of TM4C123G_Launchpad_Workshop under CCS_ver5.5. At first, I was wondering if there is any step missed; after TIVA_Ware ver1.1 installed in different location (separating from ver2.1.x) & modify the Path//Build Variables, original 5 errors were solved & Debug perspective works as expected. Could you tell us how to fix this problem if TIVA_Ware ver2.1.x is adopted (rather than ver1.1), Thank you !
Regards, William Wu
[ Console messages ]
error #16004-D: file "C:/ti/TivaWare_C_Series-2.1.1.71/driverlib/ccs/Debug/driverlib.lib<gpio.obj>" has a Tag_PCS_config attribute value of "1" that is different than one previously seen ("0"); combining incompatible files
error #16004-D: file "C:/ti/TivaWare_C_Series-2.1.1.71/driverlib/ccs/Debug/driverlib.lib<interrupt.obj>" has a Tag_PCS_config attribute value of "1" that is different than one previously seen ("0"); combining incompatible files
error #16004-D: file "C:/ti/TivaWare_C_Series-2.1.1.71/driverlib/ccs/Debug/driverlib.lib<sysctl.obj>" has a Tag_PCS_config attribute value of "1" that is different than one previously seen ("0"); combining incompatible files
>> Compilation failure
error #16004-D: file "C:/ti/TivaWare_C_Series-2.1.1.71/driverlib/ccs/Debug/driverlib.lib<cpu.obj>" has a Tag_PCS_config attribute value of "1" that is different than one previously seen ("0"); combining incompatible files
error #10010: errors encountered during linking; "lab2.out" not built