Other Parts Discussed in Thread: TMS570LS3137, HALCOGEN
I'm having a strange problem with CAN on the TMS570LS3137. Distilled to the simplest terms, I have one message box transmitting a variety of message IDs. Very rarely a message is transmitted with the correct data, but the ID from the previous transmission.
This fictitious data reflects what I have seen with both a CAN analyzer and scope:
ID Data 08000000 00 00 00 00 00 00 00 00 08000001 00 00 00 00 00 00 00 01 08000002 00 00 00 00 00 00 00 02 08000002 00 00 00 00 00 00 00 03 <- Data is correct, but ID should have been 08000003 08000004 00 00 00 00 00 00 00 04
My driver code is based on the Halcogen's canTransmit(), but modified so that ArbID and Length are updated each transmission.
/* Abort if pending message */
if ((node->TXRQx[regIndex] & bitIndex) != 0U)
{
success = 0U;
}
else
{
while ((node->IF1STAT & 0x80U) == 0x80U) { } /* Wait for IF ready */
node->IF1CMD = 0xB7u; /* Write DATA, ARB & MCTL */
node->IF1MCTL = 0x0880 | length; /* E0B, TxIE & length */
node->IF1ARB = 0xE0000000 | can_id; /* Msg Valid, Xtd, Transmit & CAN ID */
my_test[i_test].id = node->IF1ARB & 0x1FFFFFFFU; /* Diagnostic only! */
my_test[i_test].data = *(uint64_t *)data; /* Diagnostic only! */
if (i_test < MAX_TEST) { i_test++; } /* Diagnostic only! */
/* Copy TX data into IF1, converting from big endian CPU mode to little endian
* peripheral registers. */
for (i = 0U; i < length; i++)
{
node->IF1DATx[kCanByteOrder[i]] = *data;
data++;
}
node->IF1NO = (uint8)message_box; /* This write initiates IF transfer */
success = 1U;
}
With the addition of some diagnostic code I have verified that the correct ArbID and data are always loaded into the DCAN registers.
One pattern I have noticed is that the problem only occurs when there are other transmitters on the bus and arbitration is occurring. But the priority of the message does not seem to matter-- it occurs equally with very high IDs and very low IDs.
To summarize: I update MCTL, ARB and DATA with every transmission, but intermittently it appears as though the ARB was not updated.
I appreciate any and all advice.