Other Parts Discussed in Thread: TM4C123GH6PM
Hi, basically for my program it is to receive input from voltage supply (3.0V) for ADC test. UARTBufferFlag is used for further uses but right now I need to get my ADC to work.
This is my main:
#include <stdint.h>
#include <stdbool.h>
#include "inc/hw_memmap.h"
#include "inc/hw_types.h"
#include "driverlib/debug.h"
#include "driverlib/gpio.h"
#include "driverlib/pin_map.h"
#include "driverlib/sysctl.h"
#include "driverlib/adc.h"
#include "driverlib/uart.h"
#include "driverlib/interrupt.h"
#include "utils/ustdlib.h"
#include "driverlib/timer.h"
#include "UART.h"
#include "ADC.h"
#include "Timer.h"
int UARTBufferFlag = 0; // UARTBufferFlag intialise to '0' at start
/*void delay(int count){
int i, j;
for (i=0;i<count;i++)
{ for (j=0;j<1000;j++);}
}
*/
void UARTIntHandler(void)
{
uint32_t ui32Status;
ui32Status = UARTIntStatus(UART0_BASE, true); //get interrupt status
UARTIntClear(UART0_BASE, ui32Status); //clear the asserted interrupts
while(UARTCharsAvail(UART0_BASE)) //loop while there are chars
{
UARTCharPutNonBlocking(UART0_BASE, UARTCharGetNonBlocking(UART0_BASE)); //echo character
SysCtlDelay(SysCtlClockGet() / (1000 * 3)); //delay ~1 msec
}
}
int main(void) {
SysCtlClockSet(SYSCTL_SYSDIV_4 | SYSCTL_USE_PLL | SYSCTL_OSC_MAIN | SYSCTL_XTAL_16MHZ);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOB);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOF);
GPIOPinTypeGPIOOutput(GPIO_PORTF_BASE, GPIO_PIN_1);
GPIOPinTypeGPIOInput(GPIO_PORTB_BASE, GPIO_PIN_5);
GPIOPinTypeADC(GPIO_PORTB_BASE, GPIO_PIN_5);
//GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_1, 0);
Timer_Init(); // initialization of Timer
ADC_Init(); // intialization of ADC
UART_Init(); // initialization of UART
while (1)
{
if (UARTBufferFlag){// if UARTBufferFlag true
GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_1, GPIO_PIN_1);
send_uart(); // print converted ADC results through UART
UARTBufferFlag= 0; // clear UARTBufferFlag
}
//delay(100);
}
}
// end
This is my ADC.c
#include <stdint.h>
#include <stdbool.h>
#include "inc/hw_memmap.h"
#include "inc/hw_types.h"
#include "driverlib/debug.h"
#include "driverlib/gpio.h"
#include "driverlib/sysctl.h"
#include "driverlib/adc.h"
#include "ADC.h"
void ADC_Init (void) //initialization of ADC
{
SysCtlPeripheralEnable(SYSCTL_PERIPH_ADC0);
ADCSequenceConfigure(ADC0_BASE, 1, ADC_TRIGGER_PROCESSOR, 0);
ADCSequenceStepConfigure(ADC0_BASE, 1, 0, ADC_CTL_CH11);
ADCSequenceStepConfigure(ADC0_BASE, 1, 1, ADC_CTL_CH11);
ADCSequenceStepConfigure(ADC0_BASE, 1, 2, ADC_CTL_CH11);
ADCSequenceStepConfigure(ADC0_BASE,1,3,ADC_CTL_CH11|ADC_CTL_IE|ADC_CTL_END);
ADCSequenceEnable(ADC0_BASE, 1);
}
void ADCIntHandler (void) //ADC conversion
{
ADCIntClear(ADC0_BASE, 1);
ADCSequenceDataGet(ADC0_BASE, 1, ui32ADC0Value);
ui32ADC0Avg = (ui32ADC0Value[0] + ui32ADC0Value[1] + ui32ADC0Value[2] + ui32ADC0Value[3] + 2)/4;
UARTBufferFlag = 1;
}
// end
This is my timer.c
#include <stdint.h>
#include <stdbool.h>
#include "inc/tm4c123gh6pm.h"
#include "inc/hw_memmap.h"
#include "inc/hw_types.h"
#include "driverlib/sysctl.h"
#include "driverlib/interrupt.h"
#include "driverlib/adc.h"
#include "driverlib/gpio.h"
#include "driverlib/timer.h"
#include "Timer.h"
void Timer_Init (void) // initialization of Timer
{
SysCtlPeripheralEnable(SYSCTL_PERIPH_TIMER0);
TimerConfigure(TIMER0_BASE, TIMER_CFG_PERIODIC);
ui32Period = (SysCtlClockGet() / 10) / 2;
TimerLoadSet(TIMER0_BASE, TIMER_A, ui32Period -1);
IntEnable(INT_TIMER0A);
TimerIntEnable(TIMER0_BASE, TIMER_TIMA_TIMEOUT);
IntMasterEnable();
TimerEnable(TIMER0_BASE, TIMER_A);
}
void Timer0IntHandler (void) // clear interrupt and start ADC conversion
{
TimerIntClear(TIMER0_BASE, TIMER_TIMA_TIMEOUT);
ADCProcessorTrigger(ADC0_BASE, 1);
}
// end
I have even set a breakpoint on ADC.c on the "ADCIntClear(ADC0_BASE, 1);" line to test whether it will jump to the line.