Other Parts Discussed in Thread: EK-TM4C123GXL
Working with the EK-TM4C123GXL launch pad with CCS Version: 6.1.0.00104, I attempted to adapt the dead_band.c example (from Tivaware_C_Series-2.1.0.12573) to pins PF0/PF1. I see no output on the 'scope, so I am overlooking something, no doubt. Here is the code. Please advise.
#include "C:\ti\TivaWare_C_Series-2.1.1.71\driverlib\pin_map.h"
#include <stdint.h>
#include <stdbool.h>
#include "C:\ti\TivaWare_C_Series-2.1.1.71\inc\hw_gpio.h"
#include "C:\ti\TivaWare_C_Series-2.1.1.71\inc\hw_types.h"
#include "C:\ti\TivaWare_C_Series-2.1.1.71\inc\hw_memmap.h"
#include "C:\ti\TivaWare_C_Series-2.1.1.71\driverlib\sysctl.h"
#include "C:\ti\TivaWare_C_Series-2.1.1.71\driverlib\gpio.h"
#include "C:\ti\TivaWare_C_Series-2.1.1.71\driverlib\pwm.h"
int main(void)
{
//Set the clock
SysCtlClockSet(SYSCTL_SYSDIV_1 | SYSCTL_USE_OSC | SYSCTL_OSC_MAIN | SYSCTL_XTAL_16MHZ);
//Configure PWM Clock to match system
SysCtlPWMClockSet(SYSCTL_PWMDIV_1);
// Enable the peripherals used by this program.
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOF);
SysCtlPeripheralEnable(SYSCTL_PERIPH_PWM1); //The Tiva Launchpad has two modules (0 and 1).
// Unlock the Pin PF0 and Set the Commit Bit
// See datasheet table 10-1 for explanation of why this pin needs unlocking
HWREG(GPIO_PORTF_BASE + GPIO_O_LOCK) = GPIO_LOCK_KEY;
HWREG(GPIO_PORTF_BASE + GPIO_O_CR) |= 0x01;
//Configure PF0 and PF1 Pins as PWM
//See table 20-1 for these assignments
GPIOPinConfigure(GPIO_PF0_M1PWM4);
GPIOPinConfigure(GPIO_PF1_M1PWM5);
GPIOPinTypePWM(GPIO_PORTF_BASE, GPIO_PIN_0 | GPIO_PIN_1);
//Configure PWM Options:PWM_GEN_2 Covers M1PWM4 and M1PWM5
PWMGenConfigure(PWM1_BASE, PWM_GEN_2, PWM_GEN_MODE_UP_DOWN | PWM_GEN_MODE_NO_SYNC);
unsigned long period = 64000;
//Set the Period (expressed in clock ticks)
PWMGenPeriodSet(PWM1_BASE, PWM_GEN_2, period);
//Set PWM duty
PWMPulseWidthSet(PWM1_BASE, PWM_OUT_4,
PWMGenPeriodGet(PWM1_BASE, PWM_OUT_4) / 4);
PWMDeadBandEnable(PWM1_BASE, PWM_GEN_2, 160, 160);
// Turn on the Output pins
PWMOutputState(PWM1_BASE, PWM_OUT_4_BIT | PWM_OUT_5_BIT, true);
// Enable the PWM generator
PWMGenEnable(PWM1_BASE, PWM_GEN_2);
while(1)
{
}
}