Reading the NHET chapter of the TMS570LS Technical Reference, the ECMP instruction has the following description:
If the hr_lr bit is cleared, the pin action will occur after a high resolution delay from the next resolution clock. What is meant by the phrase "next resolution clock"? Is this the next "high resolution clock" or some other clock? I expect the delay to start on the next high resolution clock. Please confirm.