Other Parts Discussed in Thread: HALCOGEN, TMS570LS0332
Hi,
I am using CCS6.1, Halcogen 4.4 and Flash API 2.1.
My project is set up using FreeRTOS. I create a task, start the scheduler (so that task runs) and then I do a bunch of initialization (for spi, het, etc) including FEE. However, during the FEE initialization, part of the FreeRTOS TCB data is overwritten, including the task priority, which is being changed from 2 to 0x43410289..which causes some issues :) How can I prevent this from happening?
See screen shots below.
Thanks,
David