Hello,
I'm using TM4C1294XL Launchpad from TI.
I need 2*CAN interface and USB interface.
Tiva C Series PinMux Utility display Collision Marks when I select CAN0, CAN1 and USB0 inside of Module TreeView.
If my own board works as USB device then can I ignore those pins USB0ID and USB0VBUS.
And I want to use LQFP package.
So, is it possible to use CAN0, CAN1, USB0 (NOT Host, Device Only) together?
Thanks
Regards.