Other Parts Discussed in Thread: HALCOGEN
Hi,
I am trying to change my projects from using the 0332 Hercules to the 0432. I thought (hoped) this would be an easy process, and I could just create a new Halcogen project, and import the DIL file from the 0332. Then I could change the device in my CCS project, change the linker file, and I would be good to go.
Importing the project seemed to work well, and all of the configuration items were moved over. However, none of the code that was in the user code sections was moved over. Of course I should be able to do a compare of all the old files to the new files and move the user code sections over manually, but I have somewhere around 15 projects to convert, so this would be very tedious and error prone.
Is there a way to easily create a new 0432 project with the same Halcogen settings and user code sections as my current 0332 project has?
Thanks,
David