Other Parts Discussed in Thread: TMDX570LC43HDK, HALCOGEN
I have followed the tutorial () found on
to try to set up a simple CAN network with the 2 TMS570LC43HDK boards (
) I have.
I have managed to generate the code in halcogen and inport the files into the CCS6 project, however every time I try to build the project to run on the board I get the following error. I have attached the very simple project along with a .txt containing the full console output from the build.
My apologies if this has been asnwered before, from my research I had found similar foroum posts but none contained this exact error.
<Linking>
warning #10366-D: automatic library build: using library "c:\ti\ccsv6\tools\compiler\arm_5.1.5\lib\rtsv7A8_A_be_v3_eabi.lib" for the first time, so it must be built. This may take a few minutes.
cygwin warning:
MS-DOS style path detected: C:\Users\s55296\Documents\Workspace\DCAN_TX\Debug
Preferred POSIX equivalent is: /cygdrive/c/Users/s55296/Documents/Workspace/DCAN_TX/Debug
CYGWIN environment variable option "nodosfilewarning" turns off this warning.
Consult the user's guide for more details about POSIX paths:

cygwin warning:
MS-DOS style path detected: C:\Users\s55296\Documents\Workspace\DCAN_TX\Debug
Preferred POSIX equivalent is: /cygdrive/c/Users/s55296/Documents/Workspace/DCAN_TX/Debug
CYGWIN environment variable option "nodosfilewarning" turns off this warning.
Consult the user's guide for more details about POSIX paths:

cygwin warning:
MS-DOS style path detected: C:\Users\s55296\Documents\Workspace\DCAN_TX\Debug
Preferred POSIX equivalent is: /cygdrive/c/Users/s55296/Documents/Workspace/DCAN_TX/Debug
CYGWIN environment variable option "nodosfilewarning" turns off this warning.
Consult the user's guide for more details about POSIX paths:

--> error: '*.obj
' not found
gmake.exe[1]: *** [library] Error 1
>> ERROR: mklib: gmake error during rtsv7A8_A_be_v3_eabi.lib build
warning #10207-D: automatic RTS selection: resolving index library "libc.a" to "c:\ti\ccsv6\tools\compiler\arm_5.1.5\lib\rtsv7A8_A_be_v3_eabi.lib", but "c:\ti\ccsv6\tools\compiler\arm_5.1.5\lib\rtsv7A8_A_be_v3_eabi.lib" was not found
undefined first referenced
symbol in file
--------- ----------------
__TI_auto_init ./source/HL_sys_startup.obj
exit ./source/HL_sys_startup.obj
error #10234-D: unresolved symbols remain
error #10010: errors encountered during linking; "DCAN_TX.out" not built
>> Compilation failure
gmake: *** [DCAN_TX.out] Error 1
gmake: Target `all' not remade because of errors.
**** Build Finished ****