Other Parts Discussed in Thread: TM4C129XNCZAD
Hello I am using TM4c129xnczad Microcontroller. WOrking on ADC driver.
As TI-RTOS framework doesn't have any ADC example . SO i am referring tivaware library to configure ADC.
Basically i need to periodically monitor couple of voltages which is connected to ADC.
To do this i require timer to take ADC samples at an specified interval.
As i am using TI-RTOS(SYS/BIOS ) framework, can I use Hardware timer provided by TM4c129xnczad Microcontroller (i.e. TIMER 0, TIMER 1 or TIMER 2).
Or i should use RTOS driven timer API (TImer_create, timer_start etc....)...etc..
If i use RTOS driven timer API are they pointing to Hardware timer of TM4c129xnczad Microcontroller internally?
Fast response is highly appreciable...........
Thanks
Sanyam