This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TM4C123 ISO7816 mode

Hi, Everyone

I need your help.
We use TM4C123x UART ISO7816 mode.

This datasheet says TM4C support for communication with ISO7816 smart cards.
and Stop bit is 2 if ISO7816 mode is used.

I understand Tiva's frame is 

-Start bit  1 bit
-Data bit   8 bit
-Parity bit 1 bit
-Stop bit   2 bit

Total 12 bit

but ISO7816 frame is defined by total 11bit.

Can TM4C123x get 11 bit frame (stop bit is 1) if some device transmit 11bit frame?

Best Regards
Hiroyasu